This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问TMS570LS1227芯片如何进入SLEEP状态,如何WAKE UP

大家好!

有没有小伙伴使用过TMS570芯片进入SLEEP状态,并在SLEEP状态下wake up。谢谢!

    • TMS570LS12x/11x 16/32-Bit RISC Flash Microcontroller Technical Reference Manual (Rev. B)

  • 谢谢!我就是想IO 高电平中断唤醒,现在不能唤醒了。

    以下是我的睡眠代码:


    void Doze()
    {
    Flash_Sleep();
    systemREG1->GHVSRC = 0x00000000;
    systemREG1->VCLKASRC = 0x00000000;
    systemREG1->RCLKSRC = 0x00000000;

    // All clock Domains are disabled except RTI
    /** @b Initialize @b Clock @b Tree: */
    // Write to Clock Source Disable Register -
    systemREG1->CSDIS = 0xFE; // disable all clock sources except OSCIN

    /** - Disable / Enable clock domain */
    systemREG1->CDDIS = 0x0
    | (uint32)((uint32)1U << 0U ) /* GCLKOFF */
    | (uint32)((uint32)1U << 1U ) /* HCLK OFF */
    | (uint32)((uint32)1U << 2U ) /* VCLKP OFF */
    | (uint32)((uint32)1U << 3U ) /* VCLK2 OFF */
    | (uint32)((uint32)1U << 4U ) /* AVCLK 1 OFF */
    | (uint32)((uint32)1U << 5U ) /* AVCLK 2 OFF */
    | (uint32)((uint32)1U << 8U ) /* VCLK3 OFF */
    | (uint32)((uint32)1U << 9U ) /* VCLK4 OFF */
    | (uint32)((uint32)1U << 10U) /* AVCLK 3 OFF */
    | (uint32)((uint32)1U << 11U); /* AVCLK 4 OFF */

    asm( " NOP");
    asm( " NOP");
    asm( " NOP");

    // Execute ARM instructions with IDLE cycles to trigger CPU clock stoppage
    asm( " WFI");
    asm( " NOP");
    asm( " b #-8");
    asm( " NOP");
    asm( " NOP");
    asm( " NOP");
    asm( " NOP");

    }

    这样调用Doze(); 以后,有中断产生,但是不能唤醒,请问如何唤醒,还需要配置一些寄存器吗

  • 示波器测量一下wakeup single信号

  • IO口中断电平吗?肯定有的,我在DOZE情况下连调试器,可以进中断函数,但是程序不会地继续往下走了。我想问下,是不是我得需要重新启动任务?还是系统会自动WAKE-UP继续运行?

  • #pragma WEAK(gioNotification)
    void gioNotification(gioPORT_t *port, uint32 bit)
    {
    /* enter user code between the USER CODE BEGIN and USER CODE END. */
    /* USER CODE BEGIN (19) */
    if (gioPORTA == port) {
    if(2 == bit) {
    qca_notification(gioGetBit(port, bit));
    } else if (5 == bit) {
    evcc_auxiliary_notification();
    } else {
    //do nothing
    }
    }
    /* USER CODE END */
    }

    这个是我的IO口中断函数,DOZE时候可以进这里,但我什么也没做 ,系统有个呼吸灯,但是呼吸灯不再继续闪烁了,CAN消息也不能处理,是不是就是没WAKEUP成功?

  • #pragma WEAK(gioNotification)
    void gioNotification(gioPORT_t *port, uint32 bit)
    {
    /* enter user code between the USER CODE BEGIN and USER CODE END. */
    /* USER CODE BEGIN (19) */
    if (gioPORTA == port) {
    if(2 == bit) {
    qca_notification(gioGetBit(port, bit));
    } else if (5 == bit) {
    evcc_auxiliary_notification();
    } else {
    //do nothing
    }
    }
    /* USER CODE END */
    }

    这是我的中断处理函数 , Doze下我能进到这个中断函数中来,但是can任务收不到任何信息,感觉程序没有继续运行,是不是就是没WAKEUP