如题,在使用PWM波产生AD采样的事件时,不能使AD采样。
我已经设置是AD采样换成硬件触发,PWM的SOCA使能,并且在软件触发下AD采样能够正确采样。
现在的问题是我怎么知道自己PWM波确实产生了事件,如果产生了事件为什么触发不了AD采样呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lily,
采用eTPWM硬件触发ADC采样,主要配置三点:
1, PINMUX的PINMMR,即在PINMUX页面配置使能相应外设Peripherals,并在Special Pin Muxing中使能相应的“Use Alternate ADC “Trigger Option””;
2,ETPWM的SOC Interrupt Event Selection,使能ADC SOCA,及配置SOCASEL寄存器;
3,ADC的触发源配置,即ADC1 Event Group Trigger Source的选择。
配置好以上几点后,在main()中做adcEnableNotification及adcStartConversion。举例-如下代码:
int main(void) {
/* USER CODE BEGIN (3) */
//_enable_interrupt_();
int a=0,n=1;
adcInit();
etpwmInit();
adcEnableNotification(adcREG1, adcGROUP0);
/* Enable IRQ - Clear I flag in CPS register */
/* Note: This is usually done by the OS or in an svc dispatcher */
_enable_IRQ_interrupt_();
adcStartConversion(adcREG1, adcGROUP0);
while (1) {
if (flag_int_adc == 1)
a=n;
// break;
}
/* USER CODE END */
return 0;
}