This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570系列的MIBSPI接口是否可以连续无间隔的发送数据?

之前使用F2812的MCBSP接口与一个音频芯片通信时,MCBSP接口的数据是可以连续发送的。

 

以为TMS570的MIBSPI接口与F2812的MCBSP接口是兼容的。

通信时,软件连续发送数据,示波器上发现每组数据(16位)发送后,需要等2个clk之后,才能再发下一个数据。请问,是否可以将该2个clk去掉,这2个时钟还是必须的等待或准备时间?

 

PS:MIBSPI配置:主,3-pin模式;

数据格式:16位,Wdelay=0,Parity enable=未使能,16400(kHz);

TG组:分4组,每组Length=32,Buffer Mode=4(Always),Oneshot Transfer,Trigger Event=TRG_ALWAYS,Trigger Source=TRG_TICK;

x 出现错误。请重试或与管理员联系。