之前使用F2812的MCBSP接口与一个音频芯片通信时,MCBSP接口的数据是可以连续发送的。
以为TMS570的MIBSPI接口与F2812的MCBSP接口是兼容的。
通信时,软件连续发送数据,示波器上发现每组数据(16位)发送后,需要等2个clk之后,才能再发下一个数据。请问,是否可以将该2个clk去掉,这2个时钟还是必须的等待或准备时间?
PS:MIBSPI配置:主,3-pin模式;
数据格式:16位,Wdelay=0,Parity enable=未使能,16400(kHz);
TG组:分4组,每组Length=32,Buffer Mode=4(Always),Oneshot Transfer,Trigger Event=TRG_ALWAYS,Trigger Source=TRG_TICK;