请问一下支持RM46L852 HDK的RTOS有哪些?我从哪里可以获得移植相关的教程。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一下支持RM46L852 HDK的RTOS有哪些?我从哪里可以获得移植相关的教程。
对于FreeRTOS更多例子,你可以先安装安全控制器的开发工具HALCoGen
在目录Hercules\HALCoGen\v04.07.01\examples\RM46x
中,提供了2个实例演示。
example_freeRTOSBlinky
example_freeRTOSRestrictedTask
/** @example example_freeRTOSBlinky.c * This is an example which descibes the steps to create an example application which * toggles the High End Timer (HET) pin 17 (LED in USB & HDK) based on the FreeRTOS timer tick of one second. * * @b Step @b 1: * * Create a new project. * * Navigate: -> File -> New -> Project * * @image html example_createProject.jpg "Figure: Create a new Project" * * @b Step @b 2: * * Configure driver code generation: * - Enable GIO driver * - Disable others * * Navigate: -> TMS570LSxx /RM4 -> Driver Enable * * @image html example_freeRTOSBlinky_enableDrivers_TMS570LS3x-RMx.jpg "Figure: Driver Configuration" * * @b Step @b 3: * * Configure Interrupt handling: * - Enable SVC * - Enter FreeRTOS SVC handler name 'vPortSWI' * * Navigate: -> TMS570LSxx /RM4 -> Interrupts * * @image html example_freeRTOSBlinky_interrupts.jpg "Figure: Interrupt Configuration" * * @b Step @b 4: * * Configure VIM RAM: * - Enter FreeRTOS Timer Tick handler name 'vPortPreemptiveTick' at offset 0x0000000C * - Enter SSI handler name 'vPortYeildWithinAPI ' at offset 0x00000058 * * Navigate: -> TMS570LSxx /RM4 -> VIM RAM * * @image html example_freeRTOSBlinky_VimRam.jpg "Figure: VIM RAM Configuration" * * @b Step @b 5: * * Configure Vectored Interrupt Module Channels: * - Enable VIM Channel 2 * - Map VIM Channel 2 to IRQ * - Enable VIM Channel 21 * - Map VIM Channel 21 to IRQ * * Navigate: -> TMS570LSxx /RM4 -> VIM Channel 0-31 * * @image html example_freeRTOSBlinky_vimChannelView.jpg "Figure: VIM Channel Configuration" * * @b Step @b 6: * * Configure OS timer tick to 1 ms: * - Enter Tick Rate of 1000 * * Navigate: -> OS -> General * * @image html example_freeRTOSBlinky_osGeneral.jpg "Figure: OS General Configuration" * * @b Step @b 7: * * Generate code * * Navigate: -> File -> Generate Code * * @image html example_freeRTOS_generateCode.jpg "Figure: Generate Code" * * @b Step @b 8: * * Copy source code below into your application. * * The example file example_freeRTOSBlinky.c can also be found in the examples folder: ../HALCoGen/examples * * @note HALCoGen generates an enpty main function in sys_main.c, * please make sure that you link in the right main function or copy the source into the user code sections of this file. * * @note Enable GCC extension in the CCS project (Project properties -> Build -> ARM Compiler -> Advanced options -> Language options -> Enable support for GCC extensions) * */ /* * Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /* USER CODE BEGIN (0) */ /* USER CODE END */ /* Include Files */ #include "sys_common.h" #include "system.h" /* USER CODE BEGIN (1) */ /* Include FreeRTOS scheduler files */ #include "FreeRTOS.h" #include "os_task.h" /* Include HET header file - types, definitions and function declarations for system driver */ #include "het.h" #include "gio.h" /* Define Task Handles */ xTaskHandle xTask1Handle; /* Task1 */ void vTask1(void *pvParameters) { for(;;) { /* Taggle HET[1] with timer tick */ gioSetBit(hetPORT1, 17, gioGetBit(hetPORT1, 17) ^ 1); vTaskDelay(100); } } /* USER CODE END */ /** @fn void main(void) * @brief Application main function * */ /* USER CODE BEGIN (2) */ /* USER CODE END */ void main(void) { /* USER CODE BEGIN (3) */ /* Set high end timer GIO port hetPort pin direction to all output */ gioSetDirection(hetPORT1, 0xFFFFFFFF); /* Create Task 1 */ if (xTaskCreate(vTask1,"Task1", configMINIMAL_STACK_SIZE, NULL, 1, &xTask1Handle) != pdTRUE) { /* Task could not be created */ while(1); } /* Start Scheduler */ vTaskStartScheduler(); /* Run forever */ while(1); /* USER CODE END */ } /* USER CODE BEGIN (4) */ /* USER CODE END */