This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大神,
我用GCC编译器生成了bootloader,请问怎么把代码从flash拷贝到ram运行?这是我的链接脚本文件:
/*----------------------------------------------------------------------------*/ /* sys_link.ld */ /* */ /* (c) Texas Instruments 2009-2013, All rights reserved. */ /* */ /*----------------------------------------------------------------------------*/ /* Entry Point */ ENTRY(_c_int00) /* Highest address of the stack */ _estack = 0x8040000; /* end of 256K RAM */ /* Generate a link error if heap and stack don't fit into RAM */ _Min_Heap_Size = 0x400; /* required amount of heap */ /* Specify the memory areas */ MEMORY { VECTORS(rx) : ORIGIN = 0x00000000, LENGTH = 0x00000020 FLASH (rx) : ORIGIN = 0x00000020, LENGTH = (0x0017FFE0 + 0x00180000) CPU_STACK (rw) : ORIGIN = 0x08000000, LENGTH = 0x00001500 /* Stack is configured in sys_core.asm */ RAM (xrw) : ORIGIN = 0x08001500, LENGTH = 0x0003EB00 MEMORY_B1 (rx) : ORIGIN = 0x60000000, LENGTH = 0K } /* Define output sections */ SECTIONS { /* The ISR vector goes first into RAM */ .intvecs : { . = ALIGN(4); KEEP(*(.intvecs)) /* ISR vector */ . = ALIGN(4); } >VECTORS /* The program code and other data goes into RAM */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); _etext = .; /* define a global symbols at end of code */ } >FLASH /* Constant data goes into RAM */ .rodata : { . = ALIGN(4); *(.rodata) /* .rodata sections (constants, strings, etc.) */ *(.rodata*) /* .rodata* sections (constants, strings, etc.) */ . = ALIGN(4); } >FLASH .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >RAM .ARM : { __exidx_start = .; *(.ARM.exidx*) __exidx_end = .; } >FLASH .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } >FLASH .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } >FLASH .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } >FLASH /* used by the startup to initialize data */ _sidata = LOADADDR(.data); /* Initialized data sections goes into RAM, load LMA copy after code */ .data : { . = ALIGN(4); _sdata = .; /* create a global symbol at data start */ *(.data) /* .data sections */ *(.data*) /* .data* sections */ . = ALIGN(4); _edata = .; /* define a global symbol at data end */ } >RAM AT> FLASH /* Uninitialized data section */ . = ALIGN(4); .bss : { /* This is used by the startup in order to initialize the .bss secion */ _sbss = .; /* define a global symbol at bss start */ __bss_start__ = _sbss; *(.bss) *(.bss*) *(COMMON) . = ALIGN(4); _ebss = .; /* define a global symbol at bss end */ __bss_end__ = _ebss; } >RAM PROVIDE ( end = _ebss ); PROVIDE ( _end = _ebss ); /* MEMORY_bank1 section, code must be located here explicitly */ /* Example: extern int foo(void) __attribute__ ((section (".mb1text"))); */ .memory_b1_text : { *(.mb1text) /* .mb1text sections (code) */ *(.mb1text*) /* .mb1text* sections (code) */ *(.mb1rodata) /* read-only data (constants) */ *(.mb1rodata*) } >MEMORY_B1 /* Remove information from the standard libraries */ /DISCARD/ : { libc.a ( * ) libm.a ( * ) libgcc.a ( * ) } .ARM.attributes 0 : { *(.ARM.attributes) } }