This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357的代码能否在RAM中运行呢



问题1   TI提供的LC4357的CMD文件,都是在FLASH中运行,调试阶段也把代码放FLASH里面了,我改了下CMD文件,调试仿真期间,可以在RAM跑了,但    有 个小问题,就是第一次进调试模式时,加载完代码,程序就自己运行了,且运行时错误的,然后我要手动点击停止,然后再重新加载一次就能正常的在RAM运行了,这个不知道是哪里的问题

问题2  程序脱机实际运行的时候,能否把代码加载到RAM里跑,我在想,这样肯定能提高代码的运行速度。如果可以的话,该怎么操作呢,而且能实现加载一部分代码到RAM的话就更好了,毕竟RAM空间比较小,只加载比较重要的一些功能代码或者算法啥的就可以了。

  • user18914063 说:
    就是第一次进调试模式时,加载完代码,程序就自己运行了,且运行时错误的,

    请问是只有第一次这样?debug configuration 内的AUOO RUN是如何设置的呢?CCS版本是多少?运行时错误能否给出详细信息?

    user18914063 说:
    如果可以的话,该怎么操作呢,而且能实现加载一部分代码到RAM的话就更好了

    这个是可以实现的。

    链接程序cmd文件中的MEMORY命令描述目标系统的内存映射。这些内存空间用作SECTIONS命令中语句的目标。

    A SECTIONS命令描述每个命名输出节的位置,并指定将哪些输入节放入其中。 

    您可以在输出部分(例如.text ,.data )内添加命令来创建符号:_text_start,_text_end,_data_start或_data_end。当将数据从闪存复制到RAM时,这些符号将很有用。

    在您的c或asm文件中,您需要将最初存储在闪存中的代码复制到RAM。类似下面这样

    //copy the contents in .text output section from FLASH to RAM:

    extern const char _text_start, _text_end;   //created in linker ld file

    void __main (void)

    {

        memcpy(&_copy_start, &_run_start, &_copy_end - &_copy_start);

        return;

    }

    您可以参考 这个链接

  • RAM里面仿真跑的问题,是每次要进调试模式时,都是一加载,然后自己就开始运行了,运行是错误的,要手动停止,再加载才能正常跑
  • 刚你发的那个链接失效了
  • 我这边是可以直接打开的

    /***********************************************************************
    * Author         : QJ Wang. qjwang@ti.com
    * Date           : 5-25-2019
    */
    /* Copyright (C) 2013-2019 Texas Instruments Incorporated - http://www.ti.com/
     *
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    /*                                                                            */
    /*----------------------------------------------------------------------------*/
    /* USER CODE BEGIN (0) */
    /* USER CODE END */
    
    
    /*----------------------------------------------------------------------------*/
    /* Linker Settings                                                            */
    
    --retain="*(.intvecs)"
    
    /* USER CODE BEGIN (1) */
    /* USER CODE END */
    
    /*----------------------------------------------------------------------------*/
    /* Memory Map  */
    MEMORY
    {
    /* USER CODE BEGIN (2) */
    /* USER CODE END */
    
        VECTORS    (X)   : origin=0x00000000 length=0x00000020 vfill = 0xffffffff
        FLASH0     (RX)  : origin=0x00000020 length=0x001FFFE0 vfill = 0xffffffff
        FLASH1     (RX)  : origin=0x00200000 length=0x00200000 vfill = 0xffffffff
        SRAM       (RWX)  : origin=0x08002000 length=0x0002D000
        STACK      (RW)  : origin=0x08000000 length=0x00002000
    
    /* USER CODE BEGIN (3) */
    /*
        ECC_VEC (R)  : origin=0xf0400000 length=0x4 ECC={algorithm=algoL2R5F021, input_range=VECTORS }
        ECC_FLA0 (R) : origin=0xf0400000 + 0x4 length=0x3FFFC ECC={algorithm=algoL2R5F021, input_range=FLASH0 }
        ECC_FLA1 (R) : origin=0xf0440000 length=0x40000 ECC={algorithm=algoL2R5F021, input_range=FLASH1 }
    */
    #if 1
        ECC_VEC  (R) : origin=(0xf0400000 + (start(VECTORS) >> 3))
                       length=(size(VECTORS) >> 3)
                       ECC={algorithm=algoL2R5F021, input_range=VECTORS}
    
        ECC_FLA0 (R) : origin=(0xf0400000 + (start(FLASH0)  >> 3))
                       length=(size(FLASH0)  >> 3)
                       ECC={algorithm=algoL2R5F021, input_range=FLASH0 }
    
        ECC_FLA1 (R) : origin=(0xf0400000 + (start(FLASH1)  >> 3))
                       length=(size(FLASH1)  >> 3)
                       ECC={algorithm=algoL2R5F021, input_range=FLASH1 }
    #endif
    /* USER CODE END */
    
    }
    
    /* USER CODE BEGIN (4) */
    ECC
    {
        algoL2R5F021 : address_mask = 0xfffffff8 /* Address Bits 31:3 */
                       hamming_mask = R4         /* Use R4/R5 build in Mask */
                       parity_mask  = 0x0c       /* Set which ECC bits are Even and Odd parity */
                       mirroring    = F021       /* RM57Lx and TMS570LCx are build in F021 */
    }
    /* USER CODE END */
    
    /*----------------------------------------------------------------------------*/
    /* Section Configuration                                                      */
    SECTIONS
    {
    /* USER CODE BEGIN (5) */
    /* USER CODE END */
       .intvecs : {} > VECTORS
    
       /* The toot directory is \Debug */
       flashAPI:
       {
         .\source\Fapi_UserDefinedFunctions.obj (.text)
         .\source\bl_flash.obj (.text)
         --library= "c:\ti\Hercules\F021 Flash API\02.01.01\F021_API_CortexR4_BE_L2FMC.lib" (.text)
       } palign=8 load = FLASH0 |FLASH1, run = SRAM, LOAD_START(apiLoadStart), RUN_START(apiRunStart), SIZE(apiLoadSize)
    
       .text    : {} palign=8 > FLASH0 |FLASH1 /*Initialized executable code and constants*/
       .const   : {} palign=8 load=FLASH0 |FLASH1, run = SRAM, LOAD_START(constLoadStart), RUN_START(constRunStart), SIZE(constLoadSize)   /*Initialized constant data (e.g. const flash_sectors[..] = )*/
       .cinit   : {} palign=8 > FLASH0 |FLASH1   /*Initialized global and static variables*/
       .pinit   : {} palign=8 > FLASH0 |FLASH1
       .data    : {} > SRAM
       .bss     : {} > SRAM
       .sysmem  : {} > SRAM
    
    /* USER CODE BEGIN (6) */
    
    /* USER CODE END */
    }
    
    /* USER CODE BEGIN (7) */
    /* USER CODE END */
    
    
    /*----------------------------------------------------------------------------*/
    /* Misc                                                                       */
    
    /* USER CODE BEGIN (8) */
    /* USER CODE END */
    /*----------------------------------------------------------------------------*/
    
    

  • debug configuration 内的AUOO RUN是如何设置的呢?CCS版本是多少?运行时错误能否给出详细信息或截图?
  • 这是我的ATUO RUN设置,CCS是9.0版本的
  • 图片未能成功上传,请您以附件形式上传,谢谢
  • 你贴出来的CMD文件,让代码在RAM中跑,那程序那边是否还要做个memcopy的调用呢
  • 1 auto run 看起来设置没有问题. “运行是错误的” 具体表现是什么?

    2 理论上程序还是需要调用memcopy
  •  程序运行是错误的,这个我可能没表述清楚,我截图了,就是上面这个截图,本来加载完毕,还要点击三角形的运行按钮才开始程序运行的,但是一加载完毕,就自己开始运行了,而且看样子应该不是在正常的运行

  • 目前我的CMD文件配置如下:

    MEMORY
    {

    FLASH0 (RX) : origin=0x00000000 length=0x00200000
    FLASH1 (RX) : origin=0x00200000 length=0x00200000

    STACKS (RW) : origin=0x08000000 length=0x00001500
    VECTORS (X) : origin=0x08001500 length=0x00000020
    RAM (RW) : origin=0x08001520 length=0x0007EA80
    }

    SECTIONS
    {


    .intvecs : {} > VECTORS
    //.text align(32) : {} > RAM//FLASH0 | FLASH1
    //.const align(32) : {} > RAM//FLASH0 | FLASH1
    .text : {} > RAM//FLASH0 | FLASH1
    .const : {} > RAM//FLASH0 | FLASH1

    //.const align(32) : {} > RAM1
    //.cinit align(32) : {} > RAM//FLASH0 | FLASH1
    //.pinit align(32) : {} > RAM//FLASH0 | FLASH1
    .cinit : {} > RAM//FLASH0 | FLASH1
    .pinit : {} > RAM//FLASH0 | FLASH1
    .bss : {} > RAM
    .data : {} > RAM
    .sysmem : {} > RAM
    }
    这个配置,在今天上午的时候,还正常的跑过几次调试模式,后来不知道哪没对,就不行了,调试模式运行明显有问题,是不是还是CMD配置有问题?我的主要目的就是想在调试阶段让代码在RAM运行,而不是每次都烧写FLASH
  • 很抱歉,之前漏掉了您的回复。请问您现在该问题如何了?