This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SafetyMCU_Bootloader这个代码包怎么配置呢?导入CCS5.4总不能正常编译



从官网下PDF手册,里面有这个代码包的链接。下下来以后导入时候提示要求ARMv5.1的编译器,我在CCS5.4中下载了5.1.7。之后导入已存在的工程后,设置为Release模式,然后把Include Options里的路径也改到了当前的目录下,但编译总是各种错。

还有就是那个F021的FLASH API,也下载了给了路径。官网的F021 FLASH API有两个,一个叫F021的,一个是C2000的,后来发现SafetyMCU_Bootloader里要用的是C2000开头的那个。这个东东能给我讲解下吗,谢谢!

各种办法都试了,总不行,例如这次是报这个错:

还有的是报require gcc extension enable。请问这个选项在CCS5.4中的哪里开启呢?

实在搞不定了,求帮助