This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570 FEE 問題

Other Parts Discussed in Thread: HALCOGEN

Dear all,

我目前正在执行FEE的测试,主要是希望达成透过FEE写值和读值。

目前我大概执行了两个礼拜,还是不是很清楚要如何操作。需要寻求您的协助。

问题1:FEE的function中有分为同步(Syn)和非同步(Asyn)两种,请问这是什麽意思?同步是指它跟什麽事情同步呢?

问题2:可否补充FEE除了用来写值(write),读值(read)外,还可以执行哪些指令?

问题3:假诺数据的更换,我不是用FEE,而是用原本的Flash,是否可以?若可以,相对FEE之下,是否有哪些不好的地方?

问题4:TMS570中也有POM(Parameter Overlay Module) 这个module,若是要用来做PID控制的参数调校,它是否更方便呢?

问题5: Halcogen里面有一个例程,从主程序看下来分别执行了:

1. Initialize RAM array

2. Write the block into EEP Asynchronously. Block size is configured in ti_fee_cfg.c file. Default Block size is
     8 bytes

3. Write the block into EEP Synchronously. Write will not happen since data is same. 

4. Read the block with unknown length

5. Invalidate a written block

6. Format bank 7

为何要做步骤1 (Initialize RAM array)?,它代表什麽样的功能?在哪一份文件有描述到此步骤?

我运行程序,要怎麽知道我是透过FEE做存取?验证方法为何?目前只看到Variables视窗跑出下面的数值,这要如何解读?

後续还有更多问题,先麻烦您回答以上这些。谢谢您