Other Parts Discussed in Thread: MSP430G2553
重载了printf函数,%d,%s格式都能正确输出,%f格式不能正确输出,系统不断重启,sprintf和sscanf中%s均不能正确执行,已经在Library Function Assumptions中设置Level of printf为full。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2553
重载了printf函数,%d,%s格式都能正确输出,%f格式不能正确输出,系统不断重启,sprintf和sscanf中%s均不能正确执行,已经在Library Function Assumptions中设置Level of printf为full。
#define UART_PRINTF
#ifdef UART_PRINTF
int fputc(int _c, register FILE *_fp);
int fputs(const char *_ptr, register FILE *_fp);
#endif
#ifdef UART_PRINTF
int fputc(int _c, register FILE *_fp)
{
UCA0TXBUF = (unsigned char) _c;
while (!(IFG2&UCA0TXIFG));
return((unsigned char)_c);
}
int fputs(const char *_ptr, register FILE *_fp)
{
unsigned int i, len;
len = strlen(_ptr);
for(i=0 ; i<len ; i++)
{
UCA0TXBUF = (unsigned char) _ptr[i];
while (!(IFG2&UCA0TXIFG));
}
return len;
}
#endif
/*
* MSP430G2553IPW20 2Kb Flash;256 Bytes RAM
*/
int main(void) {
volatile unsigned int i;
char str[16];
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
UART0_init();
LED_init();
printf("MSP430 UART printf demo\r\n");
printf("int value:%d\r\n", 125);
printf("string value:%s\r\n", "hello");
sprintf(str, "val:%f", 3.13);
printf("string value:%s\r\n", str);
// printf("float value:%.2f\r\n", 3.15);
_BIS_SR(GIE);
// while(1);
return 0;
}
以上是重载了printf中main程序的主要内容,在main函数中尝试试了几种printf的格式包括%d %s 都没问题,%f格式输出就出问题了,系统不断重启。
#include "msp430.h"
#include "stdio.h"
int putchar(int ch)
{
if(ch == '\n')
{
UCA0TXBUF = '\r';
while (!(IFG2&UCA0TXIFG));
}
UCA0TXBUF = ch;
while (!(IFG2&UCA0TXIFG));
return(ch);
}
void main()
{
float value = 123.321;
char *string = "http://www.ti.com";
WDTCTL = WDTPW + WDTHOLD;
if (CALBC1_1MHZ==0xFF) // If calibration constant erased
{
while(1); // do not load, trap CPU!!
}
DCOCTL = 0; // Select lowest DCOx and MODx settings
BCSCTL1 = CALBC1_1MHZ; // Set DCO
DCOCTL = CALDCO_1MHZ;
P1SEL = BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
P1SEL2 = BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 104; // 1MHz 9600
UCA0BR1 = 0; // 1MHz 9600
UCA0MCTL = UCBRS0; // Modulation UCBRSx = 1
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
printf("value = %f\n", value);
printf("%s\n", string);
while(1);
}