This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照操作手册《BOOST-DRV8711 》User's Guide SLVU967–May 2014进行操作;
第一步:
如图1
图1
第二步:
Select View → Target Configuration (Figure 5, left side of image)
• Right click on the User Defined folder and select New Target Configuration
如图2
图2
第三步:
选择MCU型号并保存,如图3
图3
第四步:
Go back to View → Target Configurations
如图4
图4
第五步:
Right click your newly created Target Configuration file and select Launch Selected
Configuration,
得到图5
图5
第六步:
In the Debug Menu, right click on the TI MSP430 USB1_0 connection and select Connect Target
得到图6
我的问题来了,左边显示红色字体No source available for "0xe32c" 是不是有问题呀
图6
第七步:
After the device connects, go to Run → Load → Load Program (Figure 9). Browse to the
BOOST-DRV8711 Hardware and Software Files folder that was downloaded from the tool folder.
Go into the Application subdirectory and then go into the GUI subdirectory. Select the
appProgram.out file (Application\BOOST-DRV8711_GUIvX.X\appProgram.out).
导入out文件得到图7
图7
第八步:
由第七步点OK后就得到图8
图8
图9
图9是不是显示有问题呀! 程序并没有按我的意思去跑,我想是不是哪里配置不对还是什么的,请相关技术人员帮看下,谢谢!
ComPort: Can't Initialize Target CPU: **Error**: Serial Communication failed at port: COM51, baud rate:9600! To use serial monitor, please ensure the following prerequisites are satisfied: 1. Make sure the cable is plugged into both the target and the host on the right COM port. 2. Make sure a compatible target side serial monitor is loaded and running on the target device.
你这个错误不是 CCS 导入MSP430的错误。 你能导入工程 并点小虫子图标下载么?
是不是还要配置一些东西,我debug的时候就跳出
ComPort: Can't Initialize Target CPU: **Error**: Serial Communication failed at port: COM51, baud rate:9600! To use serial monitor, please ensure the following prerequisites are satisfied: 1. Make sure the cable is plugged into both the target and the host on the right COM port. 2. Make sure a compatible target side serial monitor is loaded and running on the target device.
信息了!
我大概知道问题了
你装 . http://processors.wiki.ti.com/index.php/Category:GUI_Composer#GUI_Composer_Downloads 了没?