This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR4133 DCO精度问题

大家好,请教关于FR4133 DCO问题

以前MSP430G2xxx系列内部的DCO出厂的时候有校准,校准参数存在information memory里面,FR4133没有同样的机制吗?找了好久没看到有关于FR4133 DCO校准的说明。谢谢!

  •  4133 是通过寄存器手动设置。参考如下范例代码:

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430FR413x Demo - Configure MCLK for 8MHz sourced from DCO.
    //
    //  Description: Default DCODIV is MCLK and SMCLK source.
    //  By default, FR413x select XT1 as FLL reference.
    //  If XT1 is present, the XIN and XOUT pin needs to configure.
    //  If XT1 is absent, switch to select REFO as FLL reference automatically.
    //  XT1 is considered to be absent in this example.
    //  f(DCOCLK) = 2^FLLD * (FLLN+1) * (fFLLREFCLK / n).
    //  FLLD = 0, FLLN =243, n=1, DIVM =1, f(DCOCLK) = 2^0 * (243+1)*32768Hz = 8MHz,
    //  f(DCODIV) = (243+1)*32768Hz = 8MHz,
    //  ACLK = default REFO ~32768Hz, SMCLK = MCLK = f(DCODIV) = 8MHz.
    //  Toggle LED to indicate that the program is running.
    //
    //           MSP430FR4133
    //         ---------------
    //     /|\|               |
    //      | |               |
    //      --|RST            |
    //        |          P1.0 |---> LED
    //        |          P1.4 |---> MCLK  = 8MHz
    //        |          P8.0 |---> SMCLK = 8MHz
    //        |          P8.1 |---> ACLK  = 32768Hz
    //
    //
    //   William Goh
    //   Texas Instruments Inc.
    //   March 2014
    //   Built with IAR Embedded Workbench v6.10 & Code Composer Studio v6.0
    //******************************************************************************
    #include <msp430.h>
    
    int main(void)
    {
        WDTCTL = WDTPW | WDTHOLD;               // Stop watchdog timer
    
        __bis_SR_register(SCG0);                // disable FLL
        CSCTL3 |= SELREF__REFOCLK;              // Set REFO as FLL reference source
        CSCTL0 = 0;                             // clear DCO and MOD registers
        CSCTL1 &= ~(DCORSEL_7);                 // Clear DCO frequency select bits first
        CSCTL1 |= DCORSEL_3;                    // Set DCO = 8MHz
        CSCTL2 = FLLD_0 + 243;                  // DCODIV = 8MHz
        __delay_cycles(3);
        __bic_SR_register(SCG0);                // enable FLL
        while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
    
    
        CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                // default DCODIV as MCLK and SMCLK source
    
        P1DIR |= BIT0 | BIT4;                   // set MCLK and LED pin as output
        P1SEL0 |= BIT4;                         // set MCLK pin as second function
        P8DIR |= BIT0 | BIT1;                   // set ACLK and SMCLK pin as output
        P8SEL0 |= BIT0 | BIT1;                  // set ACLK and SMCLK pin as second function
    
        PM5CTL0 &= ~LOCKLPM5;                   // Disable the GPIO power-on default high-impedance mode
                                                // to activate previously configured port settings
    
        while(1)
        {
            P1OUT ^= BIT0;                      // Toggle P1.0 using exclusive-OR
            __delay_cycles(10000000);           // Delay for 10000000*(1/MCLK)=1.25s
        }
    }
    
  • 同时, 关于 4133 时钟的说明, 参考用户手册

    http://www.ti.com/lit/ug/slau445f/slau445f.pdf

  • 在TLV里可以找到16M 30度的校准数据,常温下的可以看下面的小注释。不过FR4133内部是集成FLL的,可以直接用了。

  • 在系列用户手册中会有说明