大家好!
我需要MSP430F5438A 与AT25DF641(Flash)SPI 模式 传输数据。对SPI模式进行了配置,根据AT25DF641(Flash)写数据的说明写了一段最简单的从flash读取数据的程序,即先传Read的opcode,再传Read的3位起始地址,再有一个Dummy Byte之类,然后说明讲在接下来时钟到来就会从Flash读出数据了。可是我的程序就是不对,我预计R6中应该每次都是FF,但是我单步调试,似乎是随机数。没有发过类似的技术咨询帖,以下把我的试验程序放在这里,请大家指导。
bis.b #0x80,&P1DIR ; Set P1.7(CS pin) to output direction
bis.b #0x80,&P1OUT
bis.b #0x31,&P3SEL ; P3.5,4,0 option select
bis.b #UCSWRST,&UCA0CTL1 ; **Reset USCI state machine**
bis.b #UCMST + UCSYNC + UCMSB,&UCA0CTL0
; 3-pin, 8-bit SPI master
; Mode 0, MSB
bis.b #UCSSEL_2,&UCA0CTL1 ; SMCLK
mov.b #0x02,&UCA0BR0 ; /2
mov.b #0x00,&UCA0BR1
mov.b #0x00,&UCA0MCTL ; No modulation
bic.b #UCSWRST,&UCA0CTL1 ;**Initialize USCI state machine**
bis.b #UCRXIE,&UCA0IE ; Enable USCI_A0 RX interrupt
Read_Flash mov.w #200,R8
bic.b #0x80,&P1OUT ; Assert CS pin to select Flash Memory
mov.b #0x0B,&UCA0TXBUF ; Send 0Bh -> TXBUF, ie. the Read Array command
Wait8 bit.b #UCTXIFG,&UCA0IFG ; USCI_A0 TX buffer ready?
jnc Wait8
mov.b #0x00,&UCA0TXBUF ; Send 3-byte Starting Address -> TXBUF
Wait9 bit.b #UCTXIFG,&UCA0IFG ; USCI_A0 TX buffer ready?
jnc Wait9
mov.b #0x00,&UCA0TXBUF
Wait10 bit.b #UCTXIFG,&UCA0IFG ; USCI_A0 TX buffer ready?
jnc Wait10
mov.b #0x00,&UCA0TXBUF
Wait11 bit.b #UCTXIFG,&UCA0IFG ; Send a Dummy Byte -> TXBUF
jnc Wait11 ; USCI_A0 TX buffer ready?
mov.b #0x00,&UCA0TXBUF
bis.w #LPM3 + GIE,SR ; Enter LPM3, enable interrupts
nop ; For debugger
;************************************************************************************
USCI_A0_ISR
;************************************************************************************
add.w &UCA0IV,PC ; Vector to interrupt handler
reti ; Vector 0: No interrupt
jmp RXIFG_HND ; Vector 2: RXIFG
reti ; Vector 4: TXIFG
RXIFG_HND
mov.b &UCA0RXBUF,R6 ; RXBUF -> R6
dec.w R8
jz Read_Finish
reti
Read_Finish bis.b #0x80,&P1OUT ; Deassert CS pin to finish the read Array command
bic.b #UCRXIE,&UCA0IE ; Enable USCI_A0 RX interrupt
reti
;************************************************************************************
; Interrupt Vectors
;************************************************************************************
.sect ".int57"
.short USCI_A0_ISR
.end