如图,CC430的收发程序,等时间长了之后,程序就飞了,一直在reset_vector中不动了,不知道是什么情况。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
/******************************************************************************
* CC430 RF Code Example - TX and RX (variable packet length =< FIFO size)
*
* Simple RF Link to Toggle Receiver's LED by pressing Transmitter's Button
* Warning: This RF code example is setup to operate at either 868 or 915 MHz,
* which might be out of allowable range of operation in certain countries.
* The frequency of operation is selectable as an active build configuration
* in the project menu.
*
* Please refer to the appropriate legal sources before performing tests with
* this code example.
*
* This code example can be loaded to 2 CC430 devices. Each device will transmit
* a small packet upon a button pressed. Each device will also toggle its LED
* upon receiving the packet.
*
* The RF packet engine settings specify variable-length-mode with CRC check
* enabled. The RX packet also appends 2 status bytes regarding CRC check, RSSI
* and LQI info. For specific register settings please refer to the comments for
* each register in RfRegSettings.c, the CC430x613x User's Guide, and/or
* SmartRF Studio.
*
* M. Morales
* Texas Instruments Inc.
* February 2010
* Built with IAR v4.21 and CCS v4.1
******************************************************************************/
#include "stdlib.h"
#include "stdio.h"
#include "../inc/RF_Toggle_LED_Demo.h"
#include "../inc/usart.h"
#include "../inc/press.h"
#include "../inc/gprs.h"
#include "../inc/time.h"
#include "../inc/ds18b20.h"
#include "cc430x613x.h"
#define PACKET_LEN (0x05) // PACKET_LEN <= 61
#define RSSI_IDX (PACKET_LEN+1) // Index of appended RSSI
#define CRC_LQI_IDX (PACKET_LEN+2) // Index of appended LQI, checksum
#define CRC_OK (BIT7) // CRC_OK bit
// 433MHz下的发射功率宏定义
#define PATABLE_VAL (0xc4) // 0XC4-- 10 dBm;
// 0X50-- 0 dBm;
// 0X2D-- -6 dBm;
// 0X26-- -12dBm;
// 0x05-- -30dBm;
// 0xc0-- max
#define LED_RBIT 6
#define LED_GBIT 7
#define LED_DIR P2DIR
#define LED_OUT P2OUT
#define LED_SEL P2SEL
#define LEDR_ON() LED_OUT|=(1<<LED_RBIT)
#define LEDG_ON() LED_OUT|=(1<<LED_GBIT)
#define LEDR_OFF() LED_OUT&=~(1<<LED_RBIT)
#define LEDG_OFF() LED_OUT&=~(1<<LED_GBIT)
#define BUTTON_BIT 0
#define BUTTON_DIR PJDIR
#define BUTTON_OUT PJOUT
#define BUTTON_REN PJREN
#define BUTTON_IN PJIN
#define WDT_ARST_20s (WDTPW+WDTCNTCL+WDTSSEL0+WDTIS2) /* 1000ms " */
extern RF_SETTINGS rfSettings;
u4 Unknow_Flg=0;
u4 Low_Flg=0;
unsigned char packetReceived;
unsigned char packetTransmit;
no_init unsigned char RxBuffer[64];
unsigned char RxBufferLength = 0;
unsigned char buttonPressed = 0;
unsigned int i = 0;
unsigned char transmitting1= 0;
unsigned char receiving = 0;
void main( void )
{// u16 press_value;
// u8 buff[10];
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD; //关闭看门狗
// WDTCTL = WDT_ARST_250;
Sys_Init();
Time_Init();
// Increase PMMCOREV level to 2 for proper radio operation
SetVCore(2); //提升内核电压 PMM Core Voltage 2 (1.75V)
ResetRadioCore(); //复位cc430 里面的Radio
InitRadio(); //初始化CC430 的Radio 模块
InitButtonLeds(); //初始化按键和LED
// Usart_Init();
// simsend_init();
// Catch_Init();
ReceiveOn(); //开启接收模式
// ReceiveOff();
P1DIR |= BIT0;
P1DIR |= BIT1;
P1DIR |= BIT2;
P1DIR |= BIT3;
P3DIR |= BIT6;
P1OUT=0x00;
P3OUT&=~BIT6;
receiving = 1;
_EINT();
P2DIR |= BIT1;
P2OUT |= BIT1;
__bis_SR_register( GIE );
// __bis_SR_register(GIE); // Enter LPM0, enable interrupts
// __no_operation(); // For debugger*/
while (1)
{
// ReceiveOn();
if(Unknow_Flg)
{
P1OUT=0X00;
Delay_ms(150);
P1OUT=0X0f;
Delay_ms(150);
}
if(Low_Flg)
{
P1OUT=0X00;
P3OUT&=~BIT6;
Delay_ms(150);
P1OUT=0X0f;
P3OUT|=BIT6;
Delay_ms(150);
}
// WDTCTL = WDT_ARST_250;
// __no_operation();
// ReceiveOn();
/* if(!(BUTTON_IN & (1<<BUTTON_BIT)))
{
// press_value=press_out();
// sprintf(buff,"5%05d",press_value);
_NOP();
delayms(30);
if(!(BUTTON_IN & (1<<BUTTON_BIT)))
{
_NOP();
LEDR_ON();
ReceiveOff();
receiving = 0;
// Transmit( (unsigned char*)buff,sizeof buff);
transmitting1= 1;
while(!(BUTTON_IN & (1<<BUTTON_BIT)));
}
}
else if(!transmitting1)
{
ReceiveOn();
receiving = 1;
}*/
}
}
void delayms(unsigned int n)
{
unsigned int i,j;
for(i=0;i<n;i++)
{
for(j=0;j<800;j++);
}
}
void InitButtonLeds(void)
{
// Initialize Port J
PJOUT = 0x01;
PJDIR = 0xFF;
// Set up the button as interruptible
BUTTON_DIR&=~(1<<BUTTON_BIT); // 按键设置为输入
BUTTON_REN|=BIT0; // 上拉
// Set up LEDs
LED_OUT&=~((1<<LED_RBIT)|(1<<LED_GBIT)); // LED端口输出0
LED_DIR|=(1<<LED_RBIT)|(1<<LED_GBIT); // LED端口方向设置为输出
}
void InitRadio(void)
{
// Set the High-Power Mode Request Enable bit so LPM3 can be entered
// with active radio enabled
PMMCTL0_H = 0xA5;
PMMCTL0_L |= PMMHPMRE_L;
PMMCTL0_H = 0x00;
WriteRfSettings(&rfSettings);
WriteSinglePATable(PATABLE_VAL);
}
void Transmit(unsigned char *buffer, unsigned char length)
{
RF1AIES |= BIT9;
RF1AIFG &= ~BIT9; // Clear pending interrupts
RF1AIE |= BIT9; // Enable TX end-of-packet interrupt
WriteBurstReg(RF_TXFIFOWR, buffer, length);
Strobe( RF_STX ); // Strobe STX
}
void ReceiveOn(void)
{
RF1AIES |= BIT9; // Falling edge of RFIFG9
RF1AIFG &= ~BIT9; // Clear a pending interrupt
RF1AIE |= BIT9; // Enable the interrupt
// Radio is in IDLE following a TX, so strobe SRX to enter Receive Mode
Strobe( RF_SRX );
}
void ReceiveOff(void)
{
RF1AIE &= ~BIT9; // Disable RX interrupts
RF1AIFG &= ~BIT9; // Clear pending IFG
// It is possible that ReceiveOff is called while radio is receiving a packet.
// Therefore, it is necessary to flush the RX FIFO after issuing IDLE strobe
// such that the RXFIFO is empty prior to receiving a packet.
Strobe( RF_SIDLE );
Strobe( RF_SFRX );
}
#pragma vector=CC1101_VECTOR
__interrupt void CC1101_ISR(void)
{
static u8 press;
_DINT();
switch(__even_in_range(RF1AIV,32)) // Prioritizing Radio Core Interrupt
{
case 0: break; // No RF core interrupt pending
case 2: break; // RFIFG0
case 4: break; // RFIFG1
case 6: break; // RFIFG2
case 8: break; // RFIFG3
case 10: break; // RFIFG4
case 12: break; // RFIFG5
case 14: break; // RFIFG6
case 16: break; // RFIFG7
case 18: break; // RFIFG8
case 20: // RFIFG9
// if(receiving) // RX end of packet
// {
// Read the length byte from the FIFO
RxBufferLength = ReadSingleReg( RXBYTES );
ReadBurstReg(RF_RXFIFORD, RxBuffer, RxBufferLength);
// Stop here to see contents of RxBuffer
__no_operation();
press=atoi(RxBuffer);
if(press==0)
{
P1OUT=0x0f;
P3OUT|=BIT6;
Unknow_Flg=0;
Low_Flg=0;
}
else if(press>0&&press<=8)
{
P1OUT=0x0f;
P3OUT&=~BIT6;
Unknow_Flg=0;
Low_Flg=0;
}
else if(press>8&&press<=16)
{
P1OUT=0x0d;
P3OUT&=~BIT6;
Unknow_Flg=0;
Low_Flg=0;
}
else if(press>16&&press<=24)
{
P1OUT=0x05;
P3OUT&=~BIT6;
Unknow_Flg=0;
Low_Flg=0;
}
else if(press>24&&press<=32)
{
P1OUT=0x04;
P3OUT&=~BIT6;
Unknow_Flg=0;
Low_Flg=0;
}
else if(press>32&&press<=40)
{
P1OUT=0x00;
P3OUT&=~BIT6;
Unknow_Flg=0;
Low_Flg=0;
}
else
{
Unknow_Flg=1;
Low_Flg=0;
}
if(press>=0&&press<=5)
{
Low_Flg=1;
Unknow_Flg=0;
}
if(RxBuffer[CRC_LQI_IDX] & CRC_OK)
{
LED_OUT |= (1<<LED_GBIT); // Toggle LED1
delayms(10);
LED_OUT &=~(1<<LED_GBIT);
}
// else while(1); // trap
break;
case 22: break; // RFIFG10
case 24: break; // RFIFG11
case 26: break; // RFIFG12
case 28: break; // RFIFG13
case 30: break; // RFIFG14
case 32: break; // RFIFG15
}
ReceiveOn();
_EINT();
__bic_SR_register_on_exit(LPM3_bits);
}
这是程序,而且当跑时间长了后会出现
Wed Jul 18 10:09:09 2012: The stack 'Stack' is filled to 92% (74 bytes used out of 80). The warning threshold is set to 90.%