MSP-EXP430G2_LaunchPad试验板能直接驱动BTL003段式液晶片吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以但是最好使用共阳极的方式,让MCU 的IO工作在拉电流方式,同时注意限流电阻最好大一点,MCU的电流承载能力很弱,单个IO不能超过6mA,整体不超过40mA(拉电流)
在这里已经有回答:www.deyisupport.com/.../11095.aspx
您好!
如果要控制BTL003的话,最少都需要16个IO,LaunchPad的IO最多也是16个,理论上讲是可行的。但是,这时候SBW接口和IO口复用,要考虑信号冲突的问题。
如果是拿来学习的话,可以尝试做做。
实际的项目的话,建议采用IO口多的芯片来做。