This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430读写info flash

Other Parts Discussed in Thread: MSP430F4152

msp430f4152的datasheet里有句话说, The flash timing generator operating frequency, fFTG, must be in the range from ~ 257 kHz to ~ 476 kHz,这个意思是由FSSELx选定的时钟频率必须在这个区间,擦写FLASH操作才能稳定进行是吗?

  • 是的。由这两个寄存器配置时钟频率

    FSSELx:时钟模式 FNx:时钟分频

  • 感谢回答。那么我在低功耗应用场合外接32k晶振作为时钟,如何得到合适的频率范围呢?

  • 感谢回答。那么我在低功耗应用场合外接32k晶振作为时钟,如何得到合适的频率范围呢?

  • 可以参考这个例程

    //******************************************************************************
    // MSP430F41x2 Demo - Flash In-System Programming, Copy SegC to SegD
    //
    // Description: This program first erases flash seg C, then it increments all
    // values in seg C, then it erases seg D, then copies seg C to seg D.
    // ACLK = n/a, MCLK = SMCLK = CALxxx_1MHZ = 1MHz
    // //* Set Breakpoint on NOP in the Mainloop to avoid Stressing Flash *//
    //
    // MSP430F41x2
    // -----------------
    // /|\| XIN|-
    // | | |
    // --|RST XOUT|-
    // | |
    //
    // P. Thanigai
    // Texas Instruments Inc.
    // January 2009
    // Built with CCE Version: 3.1 and IAR Embedded Workbench Version: 4.11
    //******************************************************************************
    #include <msp430.h>

    char value; // 8-bit value to write to seg C

    // Function prototypes
    void write_SegC(char value);
    void copy_C2D(void);

    int main(void)
    {
    WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer

    FCTL2 = FWKEY + FSSEL0 + FN1; // MCLK/3 for Flash Timing Generator
    value = 0; // initialize value

    while(1) // Repeat forever
    {
    write_SegC(value++); // Write segment C, increment value
    copy_C2D(); // Copy segment C to D
    __no_operation(); // SET BREAKPOINT HERE
    }
    }

    void write_SegC(char value)
    {
    char *Flash_ptr; // Flash pointer
    unsigned int i;

    Flash_ptr = (char *)0x1040; // Initialize Flash pointer
    FCTL3 = FWKEY; // Clear Lock bit
    FCTL1 = FWKEY + ERASE; // Set Erase bit
    *Flash_ptr = 0; // Dummy write to erase Flash seg

    FCTL1 = FWKEY + WRT; // Set WRT bit for write operation

    for (i = 0; i < 64; i++)
    {
    *Flash_ptr++ = value; // Write value to flash
    }

    FCTL1 = FWKEY; // Clear WRT bit
    FCTL3 = FWKEY + LOCK; // Set LOCK bit
    }

    void copy_C2D(void)
    {
    char *Flash_ptrC; // Segment C pointer
    char *Flash_ptrD; // Segment D pointer
    unsigned int i;

    Flash_ptrC = (char *)0x1040; // Initialize Flash segment C ptr
    Flash_ptrD = (char *)0x1000; // Initialize Flash segment D ptr
    FCTL3 = FWKEY; // Clear Lock bit
    FCTL1 = FWKEY + ERASE; // Set Erase bit
    *Flash_ptrD = 0; // Dummy write to erase Flash seg D
    FCTL1 = FWKEY + WRT; // Set WRT bit for write operation

    for (i = 0; i < 64; i++)
    {
    *Flash_ptrD++ = *Flash_ptrC++; // copy value segment C to seg D
    }

    FCTL1 = FWKEY; // Clear WRT bit
    FCTL3 = FWKEY + LOCK; // Set LOCK bit
    }