msp430f4152的datasheet里有句话说, The flash timing generator operating frequency, fFTG, must be in the range from ~ 257 kHz to ~ 476 kHz,这个意思是由FSSELx选定的时钟频率必须在这个区间,擦写FLASH操作才能稳定进行是吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
msp430f4152的datasheet里有句话说, The flash timing generator operating frequency, fFTG, must be in the range from ~ 257 kHz to ~ 476 kHz,这个意思是由FSSELx选定的时钟频率必须在这个区间,擦写FLASH操作才能稳定进行是吗?
可以参考这个例程
//******************************************************************************
// MSP430F41x2 Demo - Flash In-System Programming, Copy SegC to SegD
//
// Description: This program first erases flash seg C, then it increments all
// values in seg C, then it erases seg D, then copies seg C to seg D.
// ACLK = n/a, MCLK = SMCLK = CALxxx_1MHZ = 1MHz
// //* Set Breakpoint on NOP in the Mainloop to avoid Stressing Flash *//
//
// MSP430F41x2
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
//
// P. Thanigai
// Texas Instruments Inc.
// January 2009
// Built with CCE Version: 3.1 and IAR Embedded Workbench Version: 4.11
//******************************************************************************
#include <msp430.h>
char value; // 8-bit value to write to seg C
// Function prototypes
void write_SegC(char value);
void copy_C2D(void);
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
FCTL2 = FWKEY + FSSEL0 + FN1; // MCLK/3 for Flash Timing Generator
value = 0; // initialize value
while(1) // Repeat forever
{
write_SegC(value++); // Write segment C, increment value
copy_C2D(); // Copy segment C to D
__no_operation(); // SET BREAKPOINT HERE
}
}
void write_SegC(char value)
{
char *Flash_ptr; // Flash pointer
unsigned int i;
Flash_ptr = (char *)0x1040; // Initialize Flash pointer
FCTL3 = FWKEY; // Clear Lock bit
FCTL1 = FWKEY + ERASE; // Set Erase bit
*Flash_ptr = 0; // Dummy write to erase Flash seg
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
for (i = 0; i < 64; i++)
{
*Flash_ptr++ = value; // Write value to flash
}
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
void copy_C2D(void)
{
char *Flash_ptrC; // Segment C pointer
char *Flash_ptrD; // Segment D pointer
unsigned int i;
Flash_ptrC = (char *)0x1040; // Initialize Flash segment C ptr
Flash_ptrD = (char *)0x1000; // Initialize Flash segment D ptr
FCTL3 = FWKEY; // Clear Lock bit
FCTL1 = FWKEY + ERASE; // Set Erase bit
*Flash_ptrD = 0; // Dummy write to erase Flash seg D
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
for (i = 0; i < 64; i++)
{
*Flash_ptrD++ = *Flash_ptrC++; // copy value segment C to seg D
}
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}