错误提示信息如下:
C:\ti\ccsv6\tools\compiler\ti-cgt-msp430_4.4.3\lib\rts430_eabi.lib<boot_special.obj>
error #10234-D: unresolved symbols remain
请问应该如何解决呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
错误提示信息如下:
C:\ti\ccsv6\tools\compiler\ti-cgt-msp430_4.4.3\lib\rts430_eabi.lib<boot_special.obj>
error #10234-D: unresolved symbols remain
请问应该如何解决呢
工程设置应该没有问题,你加一个main函数应该就可以了。我用的编译器是TI v15.12.3.LTS
#include<msp430g2553.h>
//#include <msp430.h>
void Set_TimerB_PWM(void)
{
//使用系统初始化时的默认时钟1MHz,定时器B专门用于产生PWM 波形。
TA1CTL = TASSEL_2 + MC_1 + TACLR;//使用系统次主机SMCKL、增计数模式、清楚定时器B时钟
TA1CCR0 = 5001 - 1;//在1MHz的主频率下,1*10^6/5000=200Hz的中断频率
TA1CCR1 = 3751 - 2;//当寄存器TACCR1的值小于3750时,输出口保持高电平。5000*3/4=3750,此路产生3:1的PWM波形。
TA1CCR2 = 1251 - 2;//当寄存器TACCR1的值小于1250时,输出口保持高电平。5000*1/4=1250,产生1:3的PWM波
TA1CCTL1 = OUTMOD_7;//输出模式7,计数器计数到5000计数器自动置位,无需中断服务子函数。
TA1CCTL2 = OUTMOD_7;//输出模式7,计数器计数到5000计数器自动置位,无需中断服务子函数。
P2SEL |= BIT1 + BIT5;//只有这两路可选(为什么是这两路?在G2553Datasheet中有特别指明)。做第二功能使用(PWM输出)
P1DIR |= BIT6; //电机控制口CTL//这里与本例无关
P1OUT &= ~BIT6; //start with 0 -->IN2,4为1,灭//这里与本例无关
}
int main (void)
{
while (1); // Loop
{
}
}
工程设置应该没有问题,你加一个main函数应该就可以了。我用的编译器是TI v15.12.3.LTS
#include<msp430g2553.h>
//#include <msp430.h>
void Set_TimerB_PWM(void)
{
//使用系统初始化时的默认时钟1MHz,定时器B专门用于产生PWM 波形。
TA1CTL = TASSEL_2 + MC_1 + TACLR;//使用系统次主机SMCKL、增计数模式、清楚定时器B时钟
TA1CCR0 = 5001 - 1;//在1MHz的主频率下,1*10^6/5000=200Hz的中断频率
TA1CCR1 = 3751 - 2;//当寄存器TACCR1的值小于3750时,输出口保持高电平。5000*3/4=3750,此路产生3:1的PWM波形。
TA1CCR2 = 1251 - 2;//当寄存器TACCR1的值小于1250时,输出口保持高电平。5000*1/4=1250,产生1:3的PWM波
TA1CCTL1 = OUTMOD_7;//输出模式7,计数器计数到5000计数器自动置位,无需中断服务子函数。
TA1CCTL2 = OUTMOD_7;//输出模式7,计数器计数到5000计数器自动置位,无需中断服务子函数。
P2SEL |= BIT1 + BIT5;//只有这两路可选(为什么是这两路?在G2553Datasheet中有特别指明)。做第二功能使用(PWM输出)
P1DIR |= BIT6; //电机控制口CTL//这里与本例无关
P1OUT &= ~BIT6; //start with 0 -->IN2,4为1,灭//这里与本例无关
}
int main (void)
{
while (1); // Loop
{
}
}