专家好!
以前用MSP430F4152的ADC测试电池电压很简单,只需要开通对应通道,内部有一个二分之一的分压,开通内部参考基准电压源即可测试,但现在使用FR4133却没有这个通道,请问专家怎么实现测试电池电压(DVCC)?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家好!
以前用MSP430F4152的ADC测试电池电压很简单,只需要开通对应通道,内部有一个二分之一的分压,开通内部参考基准电压源即可测试,但现在使用FR4133却没有这个通道,请问专家怎么实现测试电池电压(DVCC)?谢谢!
//******************************************************************************
// MSP430FR413x Demo - ADC, Lo_Batt, Set P1.0 if AVcc < 2.50V
//
// Description: A single sample is made on A13 (Vref) with reference set to
// DVCC. Software sets ADC10SC to start sample and conversion
// - ADC10SC automatically cleared at EOC. Once conversion is completed, the
// following equation is used to calculate DVCC = (1023 * 1.5) / adcResult.
// if DVCC is < 2.5V, P1.0 set indicating a lo_Batt condition, else reset.
//
// MSP430FR4133
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// |A13 (Vref) P1.0|-->LED
//
// William Goh
// Texas Instruments Inc.
// August 2014
// Built with IAR Embedded Workbench v5.60 & Code Composer Studio v6.0
//******************************************************************************
#include <msp430.h>
unsigned int adcResult; // Temporarily stores the ADC value
// that was read from ADCMEM0
int main(void)
{
volatile unsigned long dvccValue; // Calculated DVCC value
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P1DIR |= BIT0; // Set P1.0 to output direction
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure ADC10
ADCCTL0 &= ~ADCENC; // Disable ADC
ADCCTL0 = ADCSHT_2 | ADCON; // ADCON, S&H=16 ADC clks
ADCCTL1 = ADCSHP; // ADCCLK = MODOSC; sampling timer
ADCCTL2 = ADCRES; // 10-bit conversion results
ADCIE = ADCIE0; // Enable ADC conv complete interrupt
ADCMCTL0 = ADCINCH_13 | ADCSREF_0; // A13 ADC input select = 1.5V Ref
// Vref = DVCC
// Configure reference module located in the PMM
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
while(!(PMMCTL2 & REFGENRDY)); // Poll till internal reference settles
while(1)
{
ADCCTL0 |= ADCENC | ADCSC; // Sampling and conversion start
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0, ADC_ISR will force exit
__no_operation(); // For debug only
// To calculate DVCC, the following equation is used
// DVCC = (1023 * 1.5) / adcResult
// The following equation is modified to use only integers instead
// of using float. All results needs to be divided by 100 to obtain
// the final value.
// DVCC = (1023 * 150) / adcResult
dvccValue = ((unsigned long)1023 * (unsigned long)150) / (unsigned long) (adcResult);
if (dvccValue < 250) // DVCC > 2.50V?
P1OUT |= BIT0; // Set P1.0 LED on
else
P1OUT &= ~BIT0; // Clear P1.0 LED off
}
}
// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV, ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
adcResult = ADCMEM0; // Read ADC memory
__bic_SR_register_on_exit(LPM0_bits);// Exit from LPM
break;
default:
break;
}
}////////////////部分时钟设置////////////////////
__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source
CSCTL0 = 0; // clear DCO and MOD registers
CSCTL1 &= ~(DCORSEL_3); // Clear DCO frequency select bits first
CSCTL1 |= DCORSEL_3; // Set DCO = 8MHz
CSCTL2 = FLLD_0 + 243; // DCODIV = 8MHz 000b = fDCOCLK ÷ 1 001b = fDCOCLK ÷ 2
///////////初始化
SYSCFG2 |= ADCPCTL5 | ADCPCTL6 | ADCPCTL7;
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure ADC
ADCCTL0 |= ADCSHT_2 | ADCMSC | ADCON; // 16ADCclks, MSC, ADC ON
ADCCTL1 |= ADCSHP | ADCCONSEQ_1; // ADC clock MODCLK, sampling timer, s/w trig.,single sequence
ADCCTL2= ADCRES; // 10-bit conversion results
ADCMCTL0 |= ADCINCH_7 ;//| ADCSREF_1; // A0~2(EoS); Vref=1.5V
ADCIE |= ADCIE0;
/////////////////////AD中断//////////////////////////////////
// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
ADC_Result[AD_ch] = ADCMEM0;
if(AD_ch == 0)
{
__bic_SR_register_on_exit(LPM0_bits); // Exist LPM0
}
else
{
AD_ch--;
}
break;
default:
break;
}
}
////////////////主程序循环/////////////////////////////
while(1)
{
if(ad_flage) //定时AD循环一次 采样时间大概100mS一次 ,时间改长短都一样
{
if(AD_ch==0) //通道号为0,上次转换已结束 可以取走数据
{
ADC_Result_1[AD_number]=ADC_Result[0]; //移动数据去缓冲区
ADC_Result_2[AD_number]=ADC_Result[1];
ADC_Result_3[AD_number]=ADC_Result[2];
AD_number++;
if(AD_number>20)
{AD_number=0;AD_number_bit=1; //采样次数达到20次 可以进行数据处理
}
AD_ch=2; //开始下一个循环
ADCCTL0 |= ADCENC | ADCSC; // ADC 使能,开启转换
}
}
//******************************************************************************
// MSP430FR413x Demo - ADC, Sample A2/A1/A0, internal 1.5V Ref.
//
// Description: This example works on Sequence-of-Channels Mode.
// A2/A1/A0 is sampled 16ADCclks with reference to 1.5V.
// Internal oscillator times sample (16x) and conversion(13x).
// Inside ADC_ISR A2/A1/A0 sample value put into array ADC_Result[3].
// ACLK = default REFO ~32768Hz, MCLK = SMCLK = default DCODIV ~1MHz.
//
//
// MSP430FR4133
// -----------------
// /|\| |
// | | |
// --|RST |
// | |
// >---|P1.2/A2 |
// >---|P1.1/A1 |
// >---|P1.0/A0 |
//
//
// Wei Zhao
// Texas Instruments Inc.
// Jan 2014
// Built with IAR Embedded Workbench v5.60 & Code Composer Studio v5.5
//******************************************************************************
#include <msp430.h>
unsigned char ADC_Result[3]; // 8-bit ADC conversion result array
unsigned char i;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Configure ADC A0~2 pins
SYSCFG2 |= ADCPCTL0 | ADCPCTL1 | ADCPCTL2;
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure ADC
ADCCTL0 |= ADCSHT_2 | ADCMSC | ADCON; // 16ADCclks, MSC, ADC ON
ADCCTL1 |= ADCSHP | ADCCONSEQ_1; // ADC clock MODCLK, sampling timer, s/w trig.,single sequence
ADCCTL2 &= ~ADCRES; // 8-bit conversion results
ADCMCTL0 |= ADCINCH_2 | ADCSREF_1; // A0~2(EoS); Vref=1.5V
ADCIE |= ADCIE0; // Enable ADC conv complete interrupt
// Configure reference
PMMCTL0_H = PMMPW_H; // Unlock the PMM registers
PMMCTL2 |= INTREFEN; // Enable internal reference
__delay_cycles(400); // Delay for reference settling
__no_operation();
while(1)
{
i = 2;
while(ADCCTL1 & ADCBUSY); // Wait if ADC core is active
ADCCTL0 |= ADCENC | ADCSC; // Sampling and conversion start
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0 w/ interrupts
__no_operation(); // Only for debugger
__delay_cycles(5000);
__no_operation();
}
}
// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC_VECTOR))) ADC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
{
case ADCIV_NONE:
break;
case ADCIV_ADCOVIFG:
break;
case ADCIV_ADCTOVIFG:
break;
case ADCIV_ADCHIIFG:
break;
case ADCIV_ADCLOIFG:
break;
case ADCIV_ADCINIFG:
break;
case ADCIV_ADCIFG:
ADC_Result[i] = ADCMEM0;
if(i == 0)
{
__bic_SR_register_on_exit(LPM0_bits); // Exist LPM0
}
else
{
i--;
}
break;
default:
break;
}
}谢谢您的快速回复,您的这个例程我有,我也是在这个例程基础上改的,可以说只改了变量i (AD_ch);
SYSCFG2 |= ADCPCTL0 | ADCPCTL1 | ADCPCTL2;
(SYSCFG2 |= ADCPCTL5 | ADCPCTL6 | ADCPCTL7;)
ADCMCTL0 |= ADCINCH_2 | ADCSREF_1;
(ADCMCTL0 |= ADCINCH_7; )
主循环就按例程里的做,我定时0.5s读取
ADC_Result[0],ADC_Result[1],ADC_Result2] 去显示发现数据又刷新变化,改变A6,A7通道的取样电压值读数有变化,
A5通道做改变数据无变化,还有就是任意改变取样电压,变化的数据可能不在本通道,如ADC_Result[2]对应A7通道,改变A7
取样电压ADC_Result[1]数据变化,ADC_Result[2]数据无明显变化,尤其是改变A5通道电压ADC_Result[0]无变化,ADC_Result[1]数据变化
shuyin qin 说:您好,我用的A5-A7三个通道,最高置的A7(ADCINCH_7),例程是A0-A2 最高置的A2(ADCINCH_2),这个芯片的序列应该可以是其中的一段序列吧
貌似不可以,你可以试一下 从 A7 到 A0 , 看一下 A7 A6 A5 的值是不是就正常了