多次写入同一地址下发现数据错误,为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
flash MCU都是这样的。
如果是TI flash MCU, 内部带有information flash来存储数据,建议你用information flash 来存储数据。当然也是需要擦除。
如果是TI FRAM MCU,可以直接改写不需要擦除。
这个是对information flash 写
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//****************************************************************************
// MSP-FET430P140 Demo - Flash In-System Programming, Copy SegA to SegB
//
// Description: This program first erases flash seg A, then it increments all
// values in seg A, then it erases seg B, then copies seg A to seg B.
// Assumed MCLK 550kHz - 900kHz.
// //* Set Breakpoint on NOP in the Mainloop to avoid Stressing Flash *//
//
// MSP430F149
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
//
// M. Mitchell
// Texas Instruments Inc.
// Feb 2005
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A
//******************************************************************************
#include <msp430.h>
char value; // 8-bit value to write to segment A
// Function prototypes
void write_SegA (char value);
void copy_A2B (void);
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
FCTL2 = FWKEY + FSSEL0 + FN0; // MCLK/2 for Flash Timing Generator
value = 0; // Initialize value
while(1) // Repeat forever
{
write_SegA(value++); // Write segment A, increment value
copy_A2B(); // Copy segment A to B
__no_operation(); // SET BREAKPOINT HERE
}
}
void write_SegA (char value)
{
char *Flash_ptr; // Flash pointer
unsigned int i;
Flash_ptr = (char *) 0x1080; // Initialize Flash pointer
FCTL1 = FWKEY + ERASE; // Set Erase bit
FCTL3 = FWKEY; // Clear Lock bit
*Flash_ptr = 0; // Dummy write to erase Flash segment
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
for (i=0; i<128; i++)
{
*Flash_ptr++ = value; // Write value to flash
}
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
void copy_A2B (void)
{
char *Flash_ptrA; // Segment A pointer
char *Flash_ptrB; // Segment B pointer
unsigned int i;
Flash_ptrA = (char *) 0x1080; // Initialize Flash segment A pointer
Flash_ptrB = (char *) 0x1000; // Initialize Flash segment B pointer
FCTL1 = FWKEY + ERASE; // Set Erase bit
FCTL3 = FWKEY; // Clear Lock bit
*Flash_ptrB = 0; // Dummy write to erase Flash segment B
FCTL1 = FWKEY + WRT; // Set WRT bit for write operation
for (i=0; i<128; i++)
{
*Flash_ptrB++ = *Flash_ptrA++; // Copy value segment A to segment B
}
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY + LOCK; // Set LOCK bit
}
Information Flash 除了出厂占用的固化参数以外,就是给你存用户数据的,扇区比普通Flash小