This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6435 低功耗模式4

Other Parts Discussed in Thread: MSP430F6435

MSP430F6435 在进入低功耗模式4下  串口时钟没关闭 可以通过串口唤醒吗?

  • 根据TI官方文档描述,是可以通过串口中断唤醒的,只要串口模块接收中断使能,时钟选择SMCLK或者ACLK。

    建议使用MSP430F6435 LaunchPad具体实验一下。

    如果您认为此问题已被解答,请在“这是否解答您的问题” 后,点击“”按钮。 感谢您对TI的大力支持!

  • 如果msp430时钟没有关闭,能进入LPM4模式吗?

  • 根据上面图中的Table1.3,根据相应时钟请求情况,实际上进入的是LM0~LM3。

  • main()

    {

    int i;
    P7SEL |=0x03;
    UCSCTL3 |= SELREF__REFOCLK; //FLL 参考时钟选择REFOCLK
    UCSCTL6 &= ~(XT1OFF); // XT1 On
    UCSCTL6 |= XCAP_3; // Internal load cap
    UCSCTL6 |= XT2BYPASS; //旁路XT2,
    while(BAKCTL & LOCKBAK) // Unlock XT1 pins for operation
    BAKCTL &= ~(LOCKBAK);
    do
    {
    UCSCTL7 &= ~(DCOFFG+XT1LFOFFG+XT1HFOFFG+XT2OFFG);
    // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG; // Clear fault flags

    for (i = 0xFF; i > 0; i--); // 延时,
    }while(SFRIFG1&OFIFG) ;
    // while(UCSCTL7&XT1LFOFFG) ;
    UCSCTL4 = SELM_3 + SELS_3 +SELA_0; //MCLK=8M DCOIV,SMCLK=8M DCO,UCSCTL4 默认ACLK=XT1CLK 时钟源发生错误,ACLK会自动选择REFOCLK

    //其余时钟会选择DCO——CLK
    LPM4; //进入低功耗模式 4 可以吗?

    _NOP();

    }

    芯片MSP430F6435能进入LPM4吗?