This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430F5438A内部温度传感器问题

1、关于内部温度传感器如何使用?

2、如何将内部采集的值转化为实际的温度值?

  • mspware里有例程

    //******************************************************************************
    //  MSP430F543xA Demo - ADC12_A, Sample A10 Temp and Convert to oC and oF
    //
    //  Description: A single sample is made on A10 with reference to internal
    //  1.5V Vref. Software sets ADC12SC to start sample and conversion - ADC12SC
    //  automatically cleared at EOC. ADC12 internal oscillator times sample
    //  and conversion. In Mainloop MSP430 waits in LPM4 to save power until
    //  ADC10 conversion complete, ADC12_ISR will force exit from any LPMx in
    //  Mainloop on reti.
    //  ACLK = n/a, MCLK = SMCLK = default DCO ~ 1.045MHz, ADC12CLK = ADC12OSC
    //
    //  Uncalibrated temperature measured from device to devive will vary due to
    //  slope and offset variance from device to device - please see datasheet.
    //  Note:Use the TLV calibrated temperature to measure temperature 
    // (the TLV CALIBRATED DATA IS STORED IN THE INFORMATION SEGMENT, SEE DEVICE DATASHEET)
    //
    //                MSP430F5438A
    //             -----------------
    //         /|\|              XIN|-
    //          | |                 |
    //          --|RST          XOUT|-
    //            |                 |
    //            |A10              |
    //
    //   F. Chen
    //   Texas Instruments Inc.
    //   Dec. 2012
    //   Built with IAR Embedded Workbench Version: 5.51.1 & Code Composer Studio V5.2.1
    //******************************************************************************
    #include <msp430.h>
    
    #define CALADC12_15V_30C  *((unsigned int *)0x1A1A)   // Temperature Sensor Calibration-30 C
                                                          //See device datasheet for TLV table memory mapping
    #define CALADC12_15V_85C  *((unsigned int *)0x1A1C)   // Temperature Sensor Calibration-85 C
    
    unsigned int temp;
    volatile float temperatureDegC;
    volatile float temperatureDegF;
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      
      /* Initialize the shared reference module */ 
      REFCTL0 |= REFMSTR + REFVSEL_0 + REFON;    // Enable internal 1.5V reference
      
      /* Initialize ADC12_A */ 
      ADC12CTL0 = ADC12SHT0_8 + ADC12ON;		    // Set sample time 
      ADC12CTL1 = ADC12SHP;                     // Enable sample timer
      ADC12MCTL0 = ADC12SREF_1 + ADC12INCH_10;  // ADC input ch A10 => temp sense 
      ADC12IE = 0x001;                          // ADC_IFG upon conv result-ADCMEMO
      
      __delay_cycles(75);                       // delay to allow Ref to settle
                                                // based on default DCO frequency.
                                                // See Datasheet for typical settle
                                                // time.
      ADC12CTL0 |= ADC12ENC;
    
      while(1)
      {
        ADC12CTL0 &= ~ADC12SC; 
    	ADC12CTL0 |= ADC12SC;                   // Sampling and conversion start
    
        __bis_SR_register(LPM4_bits + GIE);     // LPM4 with interrupts enabled
        __no_operation();
    	
        // Temperature in Celsius. See the Device Descriptor Table section in the
        // System Resets, Interrupts, and Operating Modes, System Control Module
        // chapter in the device user's guide for background information on the
        // used formula.
        temperatureDegC = (float)(((long)temp - CALADC12_15V_30C) * (85 - 30)) /
                (CALADC12_15V_85C - CALADC12_15V_30C) + 30.0f;
    
        // Temperature in Fahrenheit Tf = (9/5)*Tc + 32
        temperatureDegF = temperatureDegC * 9.0f / 5.0f + 32.0f;
        
        __no_operation();                       // SET BREAKPOINT HERE
      }
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC12_VECTOR
    __interrupt void ADC12ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      switch(__even_in_range(ADC12IV,34))
      {
      case  0: break;                           // Vector  0:  No interrupt
      case  2: break;                           // Vector  2:  ADC overflow
      case  4: break;                           // Vector  4:  ADC timing overflow
      case  6:                                  // Vector  6:  ADC12IFG0
        temp = ADC12MEM0;                       // Move results, IFG is cleared
        __bic_SR_register_on_exit(LPM4_bits);   // Exit active CPU
        break;
      case  8: break;                           // Vector  8:  ADC12IFG1
      case 10: break;                           // Vector 10:  ADC12IFG2
      case 12: break;                           // Vector 12:  ADC12IFG3
      case 14: break;                           // Vector 14:  ADC12IFG4
      case 16: break;                           // Vector 16:  ADC12IFG5
      case 18: break;                           // Vector 18:  ADC12IFG6
      case 20: break;                           // Vector 20:  ADC12IFG7
      case 22: break;                           // Vector 22:  ADC12IFG8
      case 24: break;                           // Vector 24:  ADC12IFG9
      case 26: break;                           // Vector 26:  ADC12IFG10
      case 28: break;                           // Vector 28:  ADC12IFG11
      case 30: break;                           // Vector 30:  ADC12IFG12
      case 32: break;                           // Vector 32:  ADC12IFG13
      case 34: break;                           // Vector 34:  ADC12IFG14
      default: break;
      }
    }
    
  • 楼上正解,但是要注意的是片内温度传感器的精度不高,偏差也会比较大,而且测到的是片内的温度,隔着一层封装呢。

    用的时候要注意