This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp432 sdk错误

在官方SDK   rtc_c_calendar_alarm_interrupt事例中,RTC参考例程,以下几处真是难懂啊!!

到底是十六进制还是十进制??

以下是调试结果:

不懂,求解释!!

  • 你好!我来回答你吧!时间存储要按二进制存取才可以正确读出 ,这是我更具例程调试的结果,经测试可用

    Volatile RTC_C_Calendar newTime;

    const RTC_C_Calendar currentTime =
    {
    00, //秒
    06, //分
    20, //时
    00, //星期
    03, //日
    06, //月
    2018 //年
    };


    unsigned int sec ;

    void RtcInit(void){
    GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_PJ,GPIO_PIN0 | GPIO_PIN1,
    GPIO_PRIMARY_MODULE_FUNCTION);//配置外部时钟管脚

    CS_setExternalClockSourceFrequency(32768,48000000);//设置外部时钟源频率

    /* Starting LFXT in non-bypass mode without a timeout. */
    CS_startLFXT(false);

    RTC_C_initCalendar(&currentTime,RTC_C_FORMAT_BINARY );//存取时间,二进制格式

    /*闹钟时间:12:40 */
    RTC_C_setCalendarAlarm(40, 12, RTC_C_ALARMCONDITION_OFF, RTC_C_ALARMCONDITION_OFF);//设置闹钟

    /* Specify an interrupt to assert every minute */
    RTC_C_setCalendarEvent(RTC_C_CALENDAREVENT_MINUTECHANGE);//指定中断每分钟中断一次

    /* Enable interrupt for RTC Ready Status, which asserts when the RTC
    * Calendar registers are ready to read.
    * Also, enable interrupts for the Calendar alarm and Calendar event. */
    RTC_C_clearInterruptFlag(RTC_C_CLOCK_READ_READY_INTERRUPT | RTC_C_TIME_EVENT_INTERRUPT| RTC_C_CLOCK_ALARM_INTERRUPT);//选择产生中断的条件
    RTC_C_enableInterrupt( RTC_C_CLOCK_READ_READY_INTERRUPT | RTC_C_TIME_EVENT_INTERRUPT | RTC_C_CLOCK_ALARM_INTERRUPT);

    /* Start RTC Clock */
    RTC_C_startClock(); //开启RTC时钟
    Interrupt_enableInterrupt(INT_RTC_C);//使能RTC中断
    Interrupt_enableMaster();//使能中断

    }

    /* RTC ISR */
    void RTC_C_IRQHandler(void) //RTC中断函数
    {
    uint32_t status;

    status = RTC_C_getEnabledInterruptStatus();//获取RTC中断的状态
    RTC_C_clearInterruptFlag(status); //清除中断状态

    if (status & RTC_C_CLOCK_READ_READY_INTERRUPT)
    {
    newTime = RTC_C_getCalendarTime(); //获取时间
    }

    if (status & RTC_C_TIME_EVENT_INTERRUPT) //每分钟触发的事件
    {



    }

    if (status & RTC_C_CLOCK_ALARM_INTERRUPT) //到达闹钟时候 触发的事件
    {



    }

    }