This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529 内核电压和时钟的关系



/* --COPYRIGHT--,BSD_EX
 * Copyright (c) 2012, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 *******************************************************************************
 *
 *                       MSP430 CODE EXAMPLE DISCLAIMER
 *
 * MSP430 code examples are self-contained low-level programs that typically
 * demonstrate a single peripheral function or device feature in a highly
 * concise manner. For this the code may rely on the device's power-on default
 * register values and settings such as the clock configuration and care must
 * be taken when combining code from several examples to avoid potential side
 * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
 * for an API functional library-approach to peripheral configuration.
 *
 * --/COPYRIGHT--*/
//******************************************************************************
//   MSP430F552x Demo - Software Toggle P1.1 with 12MHz DCO
//
//   Description: Toggle P1.1 by xor'ing P1.1 inside of a software loop.
//   ACLK is rought out on pin P1.0, SMCLK is brought out on P2.2, and MCLK
//   is brought out on pin P7.7.
//   ACLK = REFO = 32kHz, MCLK = SMCLK = 12MHz
//
//                 MSP430F552x
//             -----------------
//         /|\|                 |
//          | |             P1.0|-->ACLK
//          --|RST          P7.7|-->MCLK
//            |             P2.2|-->SMCLK
//            |                 |
//            |             P1.1|-->Port Pin
//
//   Bhargavi Nisarga
//   Texas Instruments Inc.
//   April 2009
//   Built with CCSv4 and IAR Embedded Workbench Version: 4.21
//******************************************************************************
#include <msp430.h>
int main(void)
{
  volatile unsigned int i;
  WDTCTL = WDTPW+WDTHOLD;                   // Stop WDT
  P1DIR |= BIT1;                            // P1.1 output
  P1DIR |= BIT0;                            // ACLK set out to pins
  P1SEL |= BIT0;                           
  P2DIR |= BIT2;                            // SMCLK set out to pins
  P2SEL |= BIT2;                           
  P7DIR |= BIT7;                            // MCLK set out to pins
  P7SEL |= BIT7;
  UCSCTL3 |= SELREF_2;                      // Set DCO FLL reference = REFO
  UCSCTL4 |= SELA_2;                        // Set ACLK = REFO
  __bis_SR_register(SCG0);                  // Disable the FLL control loop
  UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx
  UCSCTL1 = DCORSEL_5;                      // Select DCO range 24MHz operation
  UCSCTL2 = FLLD_1 + 374;                   // Set DCO Multiplier for 12MHz
                                            // (N + 1) * FLLRef = Fdco
                                            // (374 + 1) * 32768 = 12MHz
                                            // Set FLL Div = fDCOCLK/2
  __bic_SR_register(SCG0);                  // Enable the FLL control loop
  // Worst-case settling time for the DCO when the DCO range bits have been
  // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
  // UG for optimization.
  // 32 x 32 x 12 MHz / 32,768 Hz = 375000 = MCLK cycles for DCO to settle
  __delay_cycles(375000);
 
  // Loop until XT1,XT2 & DCO fault flag is cleared
  do
  {
    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
                                            // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG;                      // Clear fault flags
  }while (SFRIFG1&OFIFG);                   // Test oscillator fault flag
 
  while(1)
  {
    P1OUT ^= BIT1;                          // Toggle P1.1
    __delay_cycles(600000);                 // Delay
  }
}
上面官方程序  时钟是12M,
为何没有提升内核电压,不解