This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教下MSP430G2332的逻辑电平要求电压是多少?

Other Parts Discussed in Thread: MSP430G2332

请教下MSP430G2332的逻辑电平要求电压是多少?

就是在多少电压以上,逻辑电平会判定为1,

多少电压以下,逻辑电平会判定为0;

谢谢

  • 如果是这个的话,那0.45VCC跟0.55VCC中间的数怎么办?正好处于这个中间,正式尴尬啊,估计逻辑电平得不稳定,不过超过0.25VCC也就肯定不稳定了,得想其他办法了

  • 请问你的实际电平出现了多少电压?

    另外,MCU的供电,VCC实际多少电压?

    还有,了解电压回差"input voltage hysteresis"这个参数的含义吗?

  • 使用点VCC是3.3V,实际电压出现的电压是从0.7到1.1V,有可能是从3.3V掉落回来的,也有可能是开机就这个电压

    那么上升判定为高电平的电压最小是0.45VCC=1.485V,

    判定为0低电压最大会到0.55VCC=1.815V

    回差电压的大概定义我是知道的,主要用于避免在临界时,出现微小变化,导致输出电平的反复跳变

    那我这么假设,假设我这芯片的高电平判定最低减压是1.485V,那么这个逻辑0最大的电压肯定被限制在1.485-0.3=1.185V?

    如果是这样,那我3.3V掉落回来其实还是存在一定风险性的

  • 这种电压识别用IO口结构是有风险的,只能利用比较器结构识别.因为具体电平的判别和电压变化率还有一点关系