Other Parts Discussed in Thread: MSP430G2332
请教下MSP430G2332的逻辑电平要求电压是多少?
就是在多少电压以上,逻辑电平会判定为1,
多少电压以下,逻辑电平会判定为0;
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2332
请教下MSP430G2332的逻辑电平要求电压是多少?
就是在多少电压以上,逻辑电平会判定为1,
多少电压以下,逻辑电平会判定为0;
谢谢
请问你的实际电平出现了多少电压?
另外,MCU的供电,VCC实际多少电压?
还有,了解电压回差"input voltage hysteresis"这个参数的含义吗?
使用点VCC是3.3V,实际电压出现的电压是从0.7到1.1V,有可能是从3.3V掉落回来的,也有可能是开机就这个电压
那么上升判定为高电平的电压最小是0.45VCC=1.485V,
判定为0低电压最大会到0.55VCC=1.815V
回差电压的大概定义我是知道的,主要用于避免在临界时,出现微小变化,导致输出电平的反复跳变
那我这么假设,假设我这芯片的高电平判定最低减压是1.485V,那么这个逻辑0最大的电压肯定被限制在1.485-0.3=1.185V?
如果是这样,那我3.3V掉落回来其实还是存在一定风险性的