This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FRAM 存储

MSP430FR6989FRAM 存储内存里的某个数组,FRAM的地址怎么分配

  • 你的数组有多大?如果只是存储数组,这个没有太多限制,只要不和存储程序的地址冲突就可以。

  • 最大50个字节,但具体的地址能否告知哈,我在手册上没找到

  • BAORONG YANG 说:

    最大50个字节,但具体的地�能否告知哈,我在手册上没找到

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2014, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP430FR69xx Demo - Long word writes to FRAM
    //
    //   Description: Use long word write to write to 512 byte blocks of FRAM.
    //   Toggle LED after every 100 writes.
    //   NOTE: Running this example for extended periods will impact the FRAM
    //   endurance. MPU is also enabled by default in CCS.
    //   MCLK = SMCLK = default DCO
    //
    //           MSP430FR6989
    //         ---------------
    //     /|\|               |
    //      | |               |
    //      --|RST            |
    //        |               |
    //        |               |
    //        |          P1.0 |---> LED
    //
    //   Kathryn Adamsky
    //   Texas Instruments Inc.
    //   July 2016 (Updated) | April 2014 (Created)
    //   Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0
    //******************************************************************************
    #include <msp430.h>
    
    void FRAMWrite(void);
    
    #define WRITE_SIZE      128
    
    unsigned char count = 0;
    unsigned long data;
    
    #if defined(__TI_COMPILER_VERSION__)
    #pragma NOINIT(FRAM_write)
    unsigned long FRAM_write[WRITE_SIZE] ;
    #elif defined(__IAR_SYSTEMS_ICC__)
    __persistent unsigned long FRAM_write[WRITE_SIZE] = {0};
    #else
    #error Compiler not supported!
    #endif
    
    int main(void)
    {
      WDTCTL = WDTPW | WDTHOLD;                 // Stop WDT
    
      // Configure GPIO
      P1OUT &= ~BIT0;                           // Clear P1.0 output latch for a defined power-on state
      P1DIR |= BIT0;                            // Set P1.0 to output direction
    
      // Disable the GPIO power-on default high-impedance mode to activate
      // previously configured port settings
      PM5CTL0 &= ~LOCKLPM5;
    
      // Initialize dummy data
      data = 0x00010001;
    
      while(1)
      {
        data += 0x00010001;
        FRAMWrite();                            // Endless loop
        count++;
        if (count > 100)
        {
          P1OUT ^= 0x01;                        // Toggle LED to show 512K bytes
          count = 0;                            // ..have been written
          data = 0x00010001;
        }
      }
    }
    
    void FRAMWrite(void)
    {
      unsigned int i=0;
    
      for ( i= 0; i<128; i++)
      {
          FRAM_write[i] = data;
      }
    }