MSP430FR6989FRAM 存储内存里的某个数组,FRAM的地址怎么分配
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BAORONG YANG 说:最大50个字节,但具体的地�能否告知哈,我在手册上没找到
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2014, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR69xx Demo - Long word writes to FRAM
//
// Description: Use long word write to write to 512 byte blocks of FRAM.
// Toggle LED after every 100 writes.
// NOTE: Running this example for extended periods will impact the FRAM
// endurance. MPU is also enabled by default in CCS.
// MCLK = SMCLK = default DCO
//
// MSP430FR6989
// ---------------
// /|\| |
// | | |
// --|RST |
// | |
// | |
// | P1.0 |---> LED
//
// Kathryn Adamsky
// Texas Instruments Inc.
// July 2016 (Updated) | April 2014 (Created)
// Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0
//******************************************************************************
#include <msp430.h>
void FRAMWrite(void);
#define WRITE_SIZE 128
unsigned char count = 0;
unsigned long data;
#if defined(__TI_COMPILER_VERSION__)
#pragma NOINIT(FRAM_write)
unsigned long FRAM_write[WRITE_SIZE] ;
#elif defined(__IAR_SYSTEMS_ICC__)
__persistent unsigned long FRAM_write[WRITE_SIZE] = {0};
#else
#error Compiler not supported!
#endif
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// Configure GPIO
P1OUT &= ~BIT0; // Clear P1.0 output latch for a defined power-on state
P1DIR |= BIT0; // Set P1.0 to output direction
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Initialize dummy data
data = 0x00010001;
while(1)
{
data += 0x00010001;
FRAMWrite(); // Endless loop
count++;
if (count > 100)
{
P1OUT ^= 0x01; // Toggle LED to show 512K bytes
count = 0; // ..have been written
data = 0x00010001;
}
}
}
void FRAMWrite(void)
{
unsigned int i=0;
for ( i= 0; i<128; i++)
{
FRAM_write[i] = data;
}
}