This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCLK problem using MSP430F2132IPW



in this product a TI MICRO (Mfgr part#: MSP430F2132IRHBR; HW part# 300-02087LF) is used that I am using on my prototype as well. Actually my part is not a QFN package but is rather a TSOP package (Mfgr part #: MSP430F2132IPW; HW part# 300-05158), other than that the two TI MICROs are similar.

Via debugger I noticed that  a problem using this MICRO wherein I am unable to set the SMCLK from the external XTAL of about 4.9MHz (LFXT1). The MCLK seems to be running fine though.

SMCLK is configured to clock the timers and since SMCLK is unable to run the timers are not running. I was wondering if you could feedback and/or direct this e-mail to a person who has experience using this MICRO? I am attaching a section of my code to show how my clocks are set-up. I am also in touch with a TI FAE but so far no success on this issue. I look forward to your reply. -Thanks

void main(void)

{

  unsigned char k;

  //WDTCTL = WDT_ARST_250;   // initialize WD Time interval    

  WDTCTL = WDTPW + WDTHOLD;       // Stop watchdog timer    

   //pkat - Via BCSCTL1 set LFXT1 mode to High-frequency mode since XTAL is 4.9MHz

   // Also set the ACLK divider to 1

   BCSCTL1 |= XTS;          // intialize clock registers

   //pkat - Via BCSTL2 set MCLK to LFXT1CLK (4.9MHz XTAL) and its divider to 1.

   // Also set SMCLK (that feeds the counter) to LFXT1CLK and it's divider to 1

   BCSCTL2 |= SELS + SELM1 + SELM0;  //pkat  

   //pkat - Via BCSCTL3 set the XTAL's frequency range (3MHz-16MHz option) &

   //specifiy the XCAPx capacitance since XTS=1 (high frequency mode specified in BCSCTL1)

   BCSCTL3 |= LFXT1S_2;     // pkat set BSCTL3 for 4.9MHz crystal  

//    while(IFG1 & OFIFG) IFG1 &= ~OFIFG; //pkat Orig code commented out

   do

   {

     IFG1 &= ~OFIFG; //pkat - Clear OSCFault flag

     for (int i=0xFF;i>0;i--); //pkat - give time for flag to set

   } while(IFG1 &OFIFG); //pkat OSCFlag fault still set?

   //pkat Now that the OSCFault flag is clear it is safe to select MCLK's source next

//   BCSCTL2 |= SELS+SELM1+SELM0; //pkat commented out original code

   BCSCTL2 |= SELS;   // pkat- Set SCLK = LFXT1 (safe) again

   BCSCTL2 |= SELM_3; // MCLK = LFXT1 (safe)