Other Parts Discussed in Thread: MSP430F5438A
各位大侠救命,遇到个问题:MSP430F5438A 进入LPM3后,在定时器中断中退出低功耗,无法进入主程序,然后就只能进入定时中断程序了,好像是退出不了低功耗模式。而且这种情况是偶然出现的。与变量太多有关吗?在初始化时在一个结构体前加了__no_init,不然初始化超时重启。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5438A
各位大侠救命,遇到个问题:MSP430F5438A 进入LPM3后,在定时器中断中退出低功耗,无法进入主程序,然后就只能进入定时中断程序了,好像是退出不了低功耗模式。而且这种情况是偶然出现的。与变量太多有关吗?在初始化时在一个结构体前加了__no_init,不然初始化超时重启。
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430x54x Demo - Enters LPM3 (ACLK = LFXT1)
//
// Description: Configure ACLK = LFXT1 and enters LPM3. Measure current.
// ACLK = LFXT1 = 32kHz, MCLK = SMCLK = default DCO
// Note: SVS(H,L) & SVM(H,L) not disabled
//
// MSP430x5438
// -----------------
// /|\ | XIN|-
// | | | 32kHz
// ---|RST XOUT|-
// | |
//
// W. Goh
// Texas Instruments Inc.
// April 2009
// Built with CCE Version: 3.2.2 and IAR Embedded Workbench Version: 4.11B
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
P7SEL |= 0x03; // Select XT1
UCSCTL6 &= ~(XT1OFF); // XT1 On
UCSCTL6 |= XCAP_3; // Internal load cap
// Loop until XT1,XT2 & DCO stabilizes
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
UCSCTL6 &= ~(XT1DRIVE_3); // Xtal is now stable, reduce drive
// strength
P1OUT = 0x00;
P2OUT = 0x00;
P3OUT = 0x00;
P4OUT = 0x00;
P5OUT = 0x00;
P6OUT = 0x00;
P7OUT = 0x00;
P8OUT = 0x00;
P9OUT = 0x00;
P10OUT = 0x00;
P11OUT = 0x00;
PJOUT = 0x00;
P1DIR = 0xFF;
P2DIR = 0xFF;
P3DIR = 0xFF;
P4DIR = 0xFF;
P5DIR = 0xFF;
P6DIR = 0xFF;
P7DIR = 0xFF;
P8DIR = 0xFF;
P9DIR = 0xFF;
P10DIR = 0xFF;
P11DIR = 0xFF;
PJDIR = 0xFF;
__bis_SR_register(LPM3_bits); // Enter LPM3
//可以加个延时或者用外部中断打断一下试试
LPM3_EXIT;
}
void main(void)
{
......
__low_power_mode_3();
}
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A (void)
{
TA0CCR0 =656;
if(...)
{
__low_power_mode_off_on_exit();
}
}
#pragma vector = PORT2_VECTOR
__interrupt void port2(void)
{
__low_power_mode_off_on_exit() ;
}
流程就是这样的,感谢