程序是在官方的MSP430FR57xx_adc10_10.c ----ADC10, DMA Sample A2-0, 8-bit Res, Single Sequence, DCO上做了一点点的修改的。原官方的程序能正常运行,我想使用中断的方式读取ADC转换的数据,发现不能正常运行。
程序在仿真的时候只触发了一次中断,不会自动切换到下一通道。看寄存器的值,符合切换 ADC10MSC=1 、 ADC10SHP=1 、x!=0 的条件,但是程序就是不会再触发ADC的中断。
程序:
#include <msp430.h>
unsigned int ADC_Result[3]; // ADC conversion result array
unsigned char i;
int main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
P3DIR |= BIT5 +BIT6 + BIT7; // Set LEDs to output
P3OUT |= BIT5 +BIT6 + BIT7;
// Configure ADC pins
P1SEL0 |= BIT0 + BIT1 + BIT2;
P1SEL1 |= BIT0 + BIT1 + BIT2;
// Configure ADC10
ADC10CTL0 = ADC10SHT_2 + ADC10MSC + ADC10ON;// 16ADCclks, MSC, ADC ON
ADC10CTL1 = ADC10SHP + ADC10CONSEQ_1; // sampling timer, s/w trig.,single sequence
ADC10MCTL0 =ADC10INCH_2; // A0,A1,A2(EoS), AVCC reference
ADC10IE |= ADC10IE0; // Enable ADC conv complete interrupt
for (;;)
{
i = 2;
while (ADC10CTL1 & BUSY); // Wait if ADC10 core is active
ADC10CTL0 |= ADC10ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // LPM0, ADC10_ISR will force exit
if (ADC_Result[0] < 0x1FF)
P3OUT &= ~BIT5; // Clear LED off
else
P3OUT |= BIT5; // Set LED on
if (ADC_Result[1] < 0x1FF)
P3OUT &= ~BIT6; // Clear LED off
else
P3OUT |= BIT6; // Set LED on
if (ADC_Result[2] < 0x1FF)
P3OUT &= ~BIT7; // Clear LED off
else
P3OUT |= BIT7; // Set LED on
}
}
// ADC10 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC10_VECTOR))) ADC10_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADC10IV,12))
{
case 0: break; // No interrupt
case 2: break; // conversion result overflow
case 4: break; // conversion time overflow
case 6: break; // ADC10HI
case 8: break; // ADC10LO
case 10: break; // ADC10IN
case 12:
ADC_Result[i] = ADC10MEM0;
if(i == 0)
{
__bic_SR_register_on_exit(CPUOFF);
}
else
{
i--;
}
break;
default: break;
}
}