我最近在调试MSP-DSPLib 的矩阵API,并使用LEA功能,目前矩阵的加法和减法都在自己的工程里调试成功,但是矩阵的乘法调用后计算的结果似乎不对,一直找不到原因,请高手指点一下。我用的芯片是msp430fr5992,开发环境是IAR7.10,
下面是代码截图,调用完msp_matrix_mpy_q15函数后,statu显示是MSP_SUCCESS。参数和结果见下图右侧watch 1.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我最近在调试MSP-DSPLib 的矩阵API,并使用LEA功能,目前矩阵的加法和减法都在自己的工程里调试成功,但是矩阵的乘法调用后计算的结果似乎不对,一直找不到原因,请高手指点一下。我用的芯片是msp430fr5992,开发环境是IAR7.10,
下面是代码截图,调用完msp_matrix_mpy_q15函数后,statu显示是MSP_SUCCESS。参数和结果见下图右侧watch 1.
Susan Yang:
关于矩阵的乘法今天下午我又测试了一下,再补充说明一下,希望能尽快找到问题。
矩阵相乘时调用的函数是:msp_matrix_mpy_q15,这个函数实际上在文件中有两个定义,程序是通过宏定义还选择执行哪一个。
如果定义了MSP_USE_LEA则执行代码1(暂且叫代码1吧)。如果没有定义MSP_USE_LEA,还要判断是否定义__MSP430_HAS_MPY32__,如果定义了__MSP430_HAS_MPY32__就执行代码2,否则执行代码3.
我的测试如下,
inputA[2][3]=1132 2132 132 1132 132 132
inputB[3][2]=199 299 33 44 55 66
手动计算的结果是:302884 440988 236884 352988
测试1:使用#undef MSP_USE_LEA 让程序执行代码2,执行的结果是9 13 7 10.(将手动计算的结果>>15后分别是9.24 13.45 7.22 10.77,取整后就是9 13 7 10),代码1里面没有看见将结果>>15的操作。
测试2:使用#undef MSP_USE_LEA 和#__MSP430_HAS_MPY32__让程序执行代码3,执行的结果也是9 13 7 10,但是代码3里面有将结果>>15的代码。
测试3:不用#undef命令,让程序执行代码1(具有LEA功能),执行结果是213 242 25 29。
不理解相同的入口参数,为什么代码1和代码2、3计算的结果不一致。虽然代码1里面我没有看见>>15的操作。
下面是msp_matrix_mpy_q15函数的定义,关键部分我用黑体标出来了。
#if defined(MSP_USE_LEA)
msp_status msp_matrix_mpy_q15(const msp_matrix_mpy_q15_params *params, const _q15 *srcA, const _q15 *srcB, _q15 *dst)
{
uint16_t srcARows;
uint16_t srcACols;
uint16_t srcBRows;
uint16_t srcBCols;
msp_status status;
MSP_LEA_MPYMATRIXROW_PARAMS *leaParams;
/* Initialize the row and column sizes. */
srcARows = params->srcARows;
srcACols = params->srcACols;
srcBRows = params->srcBRows;
srcBCols = params->srcBCols;
#ifndef MSP_DISABLE_DIAGNOSTICS
/* Check that column of A equals rows of B */
if (srcACols != srcBRows) {
return MSP_SIZE_ERROR;
}
/* Check that the data arrays are aligned and in a valid memory segment. */
if (!(MSP_LEA_VALID_ADDRESS(srcA, 4) &
MSP_LEA_VALID_ADDRESS(srcB, 4) &
MSP_LEA_VALID_ADDRESS(dst, 4))) {
return MSP_LEA_INVALID_ADDRESS;
}
/* Acquire lock for LEA module. */
if (!msp_lea_acquireLock()) {
return MSP_LEA_BUSY;
}
#endif //MSP_DISABLE_DIAGNOSTICS
/* Initialize LEA if it is not enabled. */
if (!(LEAPMCTL & LEACMDEN)) {
msp_lea_init();
}
/* Allocate MSP_LEA_MPYMATRIXROW_PARAMS structure. */
leaParams = (MSP_LEA_MPYMATRIXROW_PARAMS *)msp_lea_allocMemory(sizeof(MSP_LEA_MPYMATRIXROW_PARAMS)/sizeof(uint32_t));
/* Set status flag. */
status = MSP_SUCCESS;
/* Iterate through each row of srcA */
while (srcARows--) {
/* Set MSP_LEA_MPYMATRIXROW_PARAMS structure. */
leaParams->rowSize = srcBRows;
leaParams->colSize = srcBCols;
leaParams->colVector = MSP_LEA_CONVERT_ADDRESS(srcB);
leaParams->output = MSP_LEA_CONVERT_ADDRESS(dst);
/* Load source arguments to LEA. */
LEAPMS0 = MSP_LEA_CONVERT_ADDRESS(srcA);
LEAPMS1 = MSP_LEA_CONVERT_ADDRESS(leaParams);
/* Invoke the LEACMD__MPYMATRIXROW command. */
msp_lea_invokeCommand(LEACMD__MPYMATRIXROW);
#ifndef MSP_DISABLE_DIAGNOSTICS
/* Check LEA interrupt flags for any errors. */
if (msp_lea_ifg & LEACOVLIFG) {
status = MSP_LEA_COMMAND_OVERFLOW;
break;
}
else if (msp_lea_ifg & LEAOORIFG) {
status = MSP_LEA_OUT_OF_RANGE;
break;
}
else if (msp_lea_ifg & LEASDIIFG) {
status = MSP_LEA_SCALAR_INCONSISTENCY;
break;
}
#endif //MSP_DISABLE_DIAGNOSTICS
/* Increment srcA and dst pointers. */
srcA += srcACols;
dst += srcBCols;
}
/* Free MSP_LEA_MPYMATRIXROW_PARAMS structure. */
msp_lea_freeMemory(sizeof(MSP_LEA_MPYMATRIXROW_PARAMS)/sizeof(uint32_t));
/* Free lock for LEA module and return status. */
msp_lea_freeLock();
return status;
}
#else //MSP_USE_LEA
msp_status msp_matrix_mpy_q15(const msp_matrix_mpy_q15_params *params, const _q15 *srcA, const _q15 *srcB, _q15 *dst)
{
uint16_t cntr;
uint16_t srcARows;
uint16_t srcACols;
uint16_t srcBRows;
uint16_t srcBCols;
uint16_t dst_row;
uint16_t dst_col;
uint16_t row_offset;
uint16_t col_offset;
uint16_t dst_row_offset;
/* Initialize the row and column sizes. */
srcARows = params->srcARows;
srcACols = params->srcACols;
srcBRows = params->srcBRows;
srcBCols = params->srcBCols;
#ifndef MSP_DISABLE_DIAGNOSTICS
/* Check that column of A equals rows of B */
if (srcACols != srcBRows) {
return MSP_SIZE_ERROR;
}
#endif //MSP_DISABLE_DIAGNOSTICS
/* In initialize loop counters. */
cntr = 0;
dst_row = 0;
dst_col = 0;
row_offset = 0;
col_offset = 0;
dst_row_offset = 0;
#if defined(__MSP430_HAS_MPY32__)
/* If MPY32 is available save control context, set to fractional mode, set saturation mode. */
uint16_t ui16MPYState = MPY32CTL0;
MPY32CTL0 = MPYFRAC | MPYDLYWRTEN | MPYSAT;
/* Loop through all srcA rows. */
while(srcARows--) {
/* Loop through all srcB columns. */
while (dst_col < srcBCols) {
/* Reset result accumulator. */
MPY32CTL0 &= ~MPYC;
RESLO = 0; RESHI = 0;
/* Loop through all elements in srcA column and srcB row. */
while(cntr < srcACols) {
MACS = srcA[row_offset + cntr];
OP2 = srcB[col_offset + dst_col];
col_offset += srcBCols;
cntr++;
}
/* Store the result */
dst[dst_row_offset + dst_col] = RESHI;
/* Update pointers. */
dst_col++;
cntr = 0;
col_offset = 0;
}
/* Update pointers. */
dst_row++;
dst_col = 0;
row_offset += srcACols;
dst_row_offset += srcBCols;
}
/* Restore MPY32 control context, previous saturation state. */
MPY32CTL0 = ui16MPYState;
#else //__MSP430_HAS_MPY32__
_iq31 result;
/* Loop through all srcA rows. */
while(srcARows--) {
/* Loop through all srcB columns. */
while (dst_col < srcBCols) {
/* Initialize accumulator. */
result = 0;
/* Loop through all elements in srcA column and srcB row. */
while(cntr < srcACols) {
result += (_iq31)srcA[row_offset + cntr] * (_iq31)srcB[col_offset + dst_col];
col_offset += srcBCols;
cntr++;
}
/* Saturate and store the result */
dst[dst_row_offset + dst_col] = (_q15)__saturate(result >> 15, INT16_MIN, INT16_MAX);
/* Update pointers. */
dst_col++;
cntr = 0;
col_offset = 0;
}
/* Update pointers. */
dst_row++;
dst_col = 0;
row_offset += srcACols;
dst_row_offset += srcBCols;
}
#endif //__MSP430_HAS_MPY32__
return MSP_SUCCESS;
}
#endif //MSP_USE_LEA
谢谢您的转发!!
今天实在没有办法了,再结合上面两条补充测试的结果,我刚刚又把matrix_ex3_mpy_q15.c测试了一下,同时手动计算了一下结果,有了一个新的发现,就是手动计算的结果>>15,然后再下取整得到的结果和例程里面计算的结果就一致了。不是特别明白为什么?是不是这个API就是这样的,返回的结果并不是直接乘加的结果,而是>>15(缩小了32768倍)。如果真实这样,那就可以肯定这个API是没有问题了。后面我再移植到自己的工程中就有信心了。
matrix_ex3_mpy_q15.c原封不动的带入测试结果如下:
inputA:0 0 0 0 0 0 0 0 0 0
0 376 751 1125 1498 1870 2241 2611 2979 3345
1 754 1505 2253 2997 3736 4469 5195 5913 6621
1 1130 2255 3372 4477 5566 6636 7683 8704 9695
0 1505 3001 4479 5930 7345 8716 10035 11294 12486
1 1882 3745 5573 7349 9057 10681 12206 13618 14904
1 2257 4483 6649 8726 10687 12506 14159 15624 16882
1 2631 5213 7701 10050 12218 14166 15858 17264 18359
inputB:0 0 0 0 0 0 0 0 0 0 0 0
0 788 1555 2281 2947 3536 4033 4425 4702 4857 4886 4788
0 1556 2951 4042 4717 4906 4590 3801 2620 1169 -403 -1934
0 2283 4043 4877 4594 3258 1175 -1178 -3262 -4599 -4883 -4049
1 2953 4721 4596 2628 -394 -3259 -4818 -4446 -2292 780 3539
0 3543 4909 3259 -394 -3805 -4879 -2956 782 4039 4814 2631
0 4044 4595 1178 -3257 -4880 -2289 2278 4877 3264 -1168 -4592
0 4439 3807 -1174 -4815 -2957 2278 4911 1934 -3252 -4724 -801
0 4720 2629 -3256 -4443 781 4878 1936 -3800 -4053 1542 4911
0 4878 1179 -4593 -2290 4039 3266 -3250 -4052 2270 4600 -1158
result: 0 0 0 0 0 0 0 0 0 0 0 0
0 2017 1697 -96 -847 -57 566 99 -429 -123 343 133
0 4013 3383 -176 -1677 -117 1119 199 -846 -243 677 265
0 5931 5021 -221 -2456 -185 1634 298 -1235 -359 988 389
0 7739 6592 -215 -3163 -263 2097 394 -1584 -468 1267 504
0 9404 8074 -142 -3774 -353 2491 488 -1879 -567 1502 605
0 10897 9449 10 -4271 -457 2804 578 -2111 -655 1686 690
0 12190 10697 249 -4637 -576 3024 663 -2273 -729 1813 757
下面是手算结果(我只计算了前面三行):
0 0 0 0 0 0 0 0 0 0 0 0
1498 66112846 55614162 -3129664 -27747896 -1846123 18554202 3271730 -14027055 -4007295 11240494 4388397
2997 131506159 110875321 -5756628 -54927470 -3816413 36673409 6542104 -27719237 -7962487 22212368 8701666
在手算结果基础上>>15(缩小32768倍):
0 0 0 0 0 0 0 0 0 0 0 0
0.045715332 2017.603943 1697.209534 -95.50976563 -846.798584 -56.33920288 566.2293091 99.84527588 -428.0717468 -122.2929382 343.0326538 133.9232483
0.091461182 4013.249481 3383.646271 -175.6783447 -1676.253357 -116.4676819 1119.183624 199.6491699 -845.9239807 -242.9958191 677.8676758 265.553772
>>15后的结果认为下取整的结果与例程中的结果一致。