Other Parts Discussed in Thread: MSP-FET, MSP430FR2355, MSP-EXP430F5529LP, MSP-EXP430FR2355
目前在使用剛購入的EXP430FR2355進行開發
在不斷修改程序反覆 燒錄<=>測試 的過程中,某一次CCS突然就連不上MCU了,按Debug後顯示如下錯誤
Error initializing emulator:
A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps).
DO NOT UNPLUG THE INTERFACE DURING THE UPDATE.
按了Update也無用,不斷跳出相同訊息,若按Ignore則跳出
Error initializing emulator:
Could not set device Vcc
實際測量各部位電壓,發現Vcc 3.3V的部分似乎進不去MCU,
把跳線帽拆下來量測時確實可以提供3.3V輸出,但跳線帽一接上馬上降至0.2V左右。
然而若使用外部電源提供3.3V(大概沒有過載保護),MCU明顯快速發熱(很快就拔下來了)
請問這情況是這顆MCU內部已經有損壞了嗎?還是有什麼其他可能的情況?
目前都找不到相關訊息,跪求大神幫忙....
補充一下:
LaunchPad上面的LED101(紅燈)是亮的,如果把3.3V跳線帽拆下則是LED102(綠燈亮),其餘跳線帽基本都沒影響。
在用CCS Debug並Update時兩個LED會交叉閃爍一陣子=>亮綠燈=>亮紅燈(跳出上述錯誤)