This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Everyone:
我有个问题,在使用MSP430F1232的时候遇到串口通信失败,无法接收到数据的情况,板子参考TI官方的Launchpad。
代码如下:
// MSP-FET430P120 Demo - USART0, UART 9600 Echo ISR, 32kHz ACLK + DCO // // Description: Echo a received character, USART0 RX ISR at high-speed using // 32kHz XTAL and DCO. Normal operation in LMP0, DCO continuously stabilized, // interrupt driven using CCR2. DCO used for UART baud generation. On a valid // RX character, character is echoed back. // Baud rate divider with 2MHz = 2MHz/9600 ~ 208 (00D0h) // ACLK = LFXT1/8 = 32768/8, MCLK = SMCLK = UCLK0 = DCOCLK ~2MHz // //* An external 32kHz watch crystal on XIN XOUT is required for ACLK *// // MSP430F123(2) // ----------------- // /|\| XIN|- // | | | 32768Hz // --|RST XOUT|- // | | // | P3.4|------------> // | | 9600 - 8N1 // | P3.5|<------------ #include <msp430.h> #define DELTA 488 // target DCO = DELTA*(4096) ~2MHz void delayms(int t) { int i; while(t--) for(i=150;i>0;i--); //delay ms } unsigned int Compare, Oldcapture; int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT P1SEL=0; // SET P1 AS IO P1DIR=0xFF; //SET P1 DIR OUT P1OUT=0xFF; //P1 OUT VALUE P3SEL |= 0x30; // P3.4,5 = USART0 TXD/RXD BCSCTL1 |= DIVA_3; // ACLK = LFXT1CLK/8 ME2 |= UTXE0 + URXE0; // Enabled USART0 TXD/RXD UCTL0 |= CHAR; // 8-bit character UTCTL0 |= SSEL1; // UCLK = SMCLK UBR00 = 0xD0; // 2MHz 9600 UBR10 = 0x00; // UMCTL0 = 0x00; // no modulation UCTL0 &= ~SWRST; // Initalize USART state machine IE2 |= URXIE0; // Enabled USART0 RX interrupt CCTL2 = CM_1 + CCIS_1 + CAP + CCIE; // CAP, ACLK, interrupt TACTL = TASSEL_2 + MC_2 + TACLR; // SMCLK, cont-mode, clear __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupt } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USART0RX_VECTOR __interrupt void usart0_rx (void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USART0RX_VECTOR))) usart0_rx (void) #else #error Compiler not supported! #endif { while (!(IFG2 & UTXIFG0)); // USART0 TX buffer ready? TXBUF0 = RXBUF0; // RXBUF0 to TXBUF0 //while receive the data, led blink and resend data to tx. P1OUT=1; delayms(50); //delay P1OUT=0; delayms(50); //delay } // Timer_A3 Interrupt Vector (TAIV) handler #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=TIMERA1_VECTOR __interrupt void Timer_A(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMERA1_VECTOR))) Timer_A (void) #else #error Compiler not supported! #endif { switch( TAIV ) { case 2: break; // CCR1 not used case 4: { Compare = CCR2; // Get current captured SMCLK Compare = Compare - Oldcapture; // SMCLK difference Oldcapture = CCR2; // Save current captured SMCLK if (DELTA < Compare) { DCOCTL--; if (DCOCTL == 0xFF) // DCO is too fast, slow it down { if (!(BCSCTL1 == (XT2OFF + DIVA_3))) BCSCTL1--; // Did DCO role under?, Sel lower RSEL } } else { DCOCTL++; // DCO is too slow, speed it down if (DCOCTL == 0x00) { if (!(BCSCTL1 == (XT2OFF + DIVA_3 + 0x07))) BCSCTL1++; // Did DCO role over? Sel higher RSEL } } } case 10: break; // not used } }
但串口依旧无法收发数据,通过示波器测得串口通信工具发送波形如下,请TI专家帮忙分析一下,谢谢!
修改后
//ACLK=32768,
UBR00 = 0x04; // 32768/ 9600=3.41
UBR10 = 0x00; //
UMCTL0 = 0x4A; // ACLK=9600 UBR0=32768/9600=3.41 MCLK=ACLK*32=109.23KHZ UxBR1=0 UxBR0=03 UxMCTL=4A
工作电压降到2.6V,使用串口可以收发数据,但数据收发处于同步模式,无法实现异步,请问串口如何配置成异步收发模式?