Hi,Everyone:
我有个问题,在使用MSP430F1232的时候遇到串口通信失败,无法接收到数据的情况,板子参考TI官方的Launchpad。
代码如下:
// MSP-FET430P120 Demo - USART0, UART 9600 Echo ISR, 32kHz ACLK + DCO
//
// Description: Echo a received character, USART0 RX ISR at high-speed using
// 32kHz XTAL and DCO. Normal operation in LMP0, DCO continuously stabilized,
// interrupt driven using CCR2. DCO used for UART baud generation. On a valid
// RX character, character is echoed back.
// Baud rate divider with 2MHz = 2MHz/9600 ~ 208 (00D0h)
// ACLK = LFXT1/8 = 32768/8, MCLK = SMCLK = UCLK0 = DCOCLK ~2MHz
// //* An external 32kHz watch crystal on XIN XOUT is required for ACLK *//
// MSP430F123(2)
// -----------------
// /|\| XIN|-
// | | | 32768Hz
// --|RST XOUT|-
// | |
// | P3.4|------------>
// | | 9600 - 8N1
// | P3.5|<------------
#include <msp430.h>
#define DELTA 488 // target DCO = DELTA*(4096) ~2MHz
void delayms(int t)
{
int i;
while(t--)
for(i=150;i>0;i--); //delay ms
}
unsigned int Compare, Oldcapture;
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P1SEL=0; // SET P1 AS IO
P1DIR=0xFF; //SET P1 DIR OUT
P1OUT=0xFF; //P1 OUT VALUE
P3SEL |= 0x30; // P3.4,5 = USART0 TXD/RXD
BCSCTL1 |= DIVA_3; // ACLK = LFXT1CLK/8
ME2 |= UTXE0 + URXE0; // Enabled USART0 TXD/RXD
UCTL0 |= CHAR; // 8-bit character
UTCTL0 |= SSEL1; // UCLK = SMCLK
UBR00 = 0xD0; // 2MHz 9600
UBR10 = 0x00; //
UMCTL0 = 0x00; // no modulation
UCTL0 &= ~SWRST; // Initalize USART state machine
IE2 |= URXIE0; // Enabled USART0 RX interrupt
CCTL2 = CM_1 + CCIS_1 + CAP + CCIE; // CAP, ACLK, interrupt
TACTL = TASSEL_2 + MC_2 + TACLR; // SMCLK, cont-mode, clear
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupt
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USART0RX_VECTOR
__interrupt void usart0_rx (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USART0RX_VECTOR))) usart0_rx (void)
#else
#error Compiler not supported!
#endif
{
while (!(IFG2 & UTXIFG0)); // USART0 TX buffer ready?
TXBUF0 = RXBUF0; // RXBUF0 to TXBUF0
//while receive the data, led blink and resend data to tx.
P1OUT=1;
delayms(50); //delay
P1OUT=0;
delayms(50); //delay
}
// Timer_A3 Interrupt Vector (TAIV) handler
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMERA1_VECTOR
__interrupt void Timer_A(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMERA1_VECTOR))) Timer_A (void)
#else
#error Compiler not supported!
#endif
{
switch( TAIV )
{
case 2: break; // CCR1 not used
case 4:
{
Compare = CCR2; // Get current captured SMCLK
Compare = Compare - Oldcapture; // SMCLK difference
Oldcapture = CCR2; // Save current captured SMCLK
if (DELTA < Compare)
{
DCOCTL--;
if (DCOCTL == 0xFF) // DCO is too fast, slow it down
{
if (!(BCSCTL1 == (XT2OFF + DIVA_3)))
BCSCTL1--; // Did DCO role under?, Sel lower RSEL
}
}
else
{
DCOCTL++; // DCO is too slow, speed it down
if (DCOCTL == 0x00)
{
if (!(BCSCTL1 == (XT2OFF + DIVA_3 + 0x07)))
BCSCTL1++; // Did DCO role over? Sel higher RSEL
}
}
}
case 10: break; // not used
}
}
但串口依旧无法收发数据,通过示波器测得串口通信工具发送波形如下,请TI专家帮忙分析一下,谢谢!