Other Parts Discussed in Thread: MSP430FR2433
MSP430FR2433的硬件IIC怎么设置为从机400K呢?我现在这边主机是IIC的400K速率,读取数据时2433反应不过来https://e2echina.ti.com/形如图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FR2433
MSP430FR2433的硬件IIC怎么设置为从机400K呢?我现在这边主机是IIC的400K速率,读取数据时2433反应不过来https://e2echina.ti.com/形如图
你好。附件里是代码吗?下载不了。
msp430里有作为iic从机的的例程,不过不是400k,楼主参考下吧
//******************************************************************************
// MSP430FR243x Demo - eUSCI_B0 I2C Slave TX multiple bytes to MSP430 Master
//
// Description: This demo connects two MSP430's via the I2C bus. The master
// reads from the slave. This is the SLAVE code. The TX data begins at 0
// and is incremented each time it is sent. A stop condition
// is used as a trigger to initialize the outgoing data.
// The USCI_B0 TX interrupt is used to know
// when to TX.
// ACLK = default REFO ~32768Hz, MCLK = SMCLK = default DCODIV ~1MHz.
//
// *****used with "msp430fr243x_euscib0_i2c_10.c"****
//
// /|\ /|\
// MSP430FR2433 10k 10k MSP430FR2433
// slave | | master
// ----------------- | | -----------------
// | P1.2/UCB0SDA|<-|----|->|P1.2/UCB0SDA |
// | | | | |
// | | | | |
// | P1.3/UCB0SCL|<-|------>|P1.3/UCB0SCL |
// | | | |
//
// Cen Fang
// Texas Instruments Inc.
// June 2013
// Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.0.1
//******************************************************************************
#include <msp430.h>
volatile unsigned char TXData;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
// Configure GPIO
P1SEL0 |= BIT2 | BIT3; // I2C pins
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure USCI_B0 for I2C mode
UCB0CTLW0 = UCSWRST; // Software reset enabled
UCB0CTLW0 |= UCMODE_3 | UCSYNC; // I2C mode, sync mode
UCB0I2COA0 = 0x48 | UCOAEN; // own address is 0x48 + enable
UCB0CTLW0 &= ~UCSWRST; // clear reset register
UCB0IE |= UCTXIE0 | UCSTPIE; // transmit,stop interrupt enable
__bis_SR_register(LPM0_bits | GIE); // Enter LPM0 w/ interrupts
__no_operation();
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B0_VECTOR
__interrupt void USCIB0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCIB0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCB0IV, USCI_I2C_UCBIT9IFG))
{
case USCI_NONE: break; // Vector 0: No interrupts
case USCI_I2C_UCALIFG: break; // Vector 2: ALIFG
case USCI_I2C_UCNACKIFG: break; // Vector 4: NACKIFG
case USCI_I2C_UCSTTIFG: break; // Vector 6: STTIFG
case USCI_I2C_UCSTPIFG: // Vector 8: STPIFG
TXData = 0;
UCB0IFG &= ~UCSTPIFG; // Clear stop condition int flag
break;
case USCI_I2C_UCRXIFG3: break; // Vector 10: RXIFG3
case USCI_I2C_UCTXIFG3: break; // Vector 14: TXIFG3
case USCI_I2C_UCRXIFG2: break; // Vector 16: RXIFG2
case USCI_I2C_UCTXIFG2: break; // Vector 18: TXIFG2
case USCI_I2C_UCRXIFG1: break; // Vector 20: RXIFG1
case USCI_I2C_UCTXIFG1: break; // Vector 22: TXIFG1
case USCI_I2C_UCRXIFG0: break; // Vector 24: RXIFG0
case USCI_I2C_UCTXIFG0:
UCB0TXBUF = TXData++;
break; // Vector 26: TXIFG0
case USCI_I2C_UCBCNTIFG: break; // Vector 28: BCNTIFG
case USCI_I2C_UCCLTOIFG: break; // Vector 30: clock low timeout
case USCI_I2C_UCBIT9IFG: break; // Vector 32: 9th bit
default: break;
}
}