This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F4784的LCD_A控制器

Other Parts Discussed in Thread: MSP430F4784

对于MSP430F4784单片机的LCD_A控制机器如果选择LCD电压为外部的LCDCAP的话,那么LCDCAP接多大电容啊,还有对于LCD的帧频率frame文档上说参考LCD数据手册,我怎么没看见MSP430F4784上介绍帧频率frame是多少啊

  • 楼主可以参考 MSP430F4系列的 user guide:

    http://www.ti.com/lit/ug/slau056k/slau056k.pdf

    13.2 Basic Timer1 Operation
    The Basic Timer1 module can be configured as two 8-bit timers or one 16-bit
    timer with the BTCTL register. The BTCTL register is an 8-bit read/write
    register. Any read or write access must use byte instructions. The Basic
    Timer1 controls the LCD frame frequency with BTCNT1.