对于MSP430F4784单片机的LCD_A控制机器如果选择LCD电压为外部的LCDCAP的话,那么LCDCAP接多大电容啊,还有对于LCD的帧频率frame文档上说参考LCD数据手册,我怎么没看见MSP430F4784上介绍帧频率frame是多少啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于MSP430F4784单片机的LCD_A控制机器如果选择LCD电压为外部的LCDCAP的话,那么LCDCAP接多大电容啊,还有对于LCD的帧频率frame文档上说参考LCD数据手册,我怎么没看见MSP430F4784上介绍帧频率frame是多少啊
楼主可以参考 MSP430F4系列的 user guide:
http://www.ti.com/lit/ug/slau056k/slau056k.pdf
13.2 Basic Timer1 Operation
The Basic Timer1 module can be configured as two 8-bit timers or one 16-bit
timer with the BTCTL register. The BTCTL register is an 8-bit read/write
register. Any read or write access must use byte instructions. The Basic
Timer1 controls the LCD frame frequency with BTCNT1.