This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADC12EOS
序列结束。指示序列中的最后一次转换。仅当 ADC12ENC = 0 时可以修改
如果我在12通道的时候设置了ADC12EOS是否会在12通道直接结束采样
应该是可以的
测试发现A12加了ADC12EOS和A3通道加上ADC12EOS,功耗还是多了十几个微安
A12的初始化
{
while(ADC12CTL1&ADC12BUSY); /* 等待采样结束 */
/* 初始化AD引脚 */
P1SEL0 |= P1_AD_I|P3_AD_U|P1_VEREF;/*模拟*/
P1SEL1 |= P1_AD_I|P3_AD_U|P1_VEREF;
P4SEL0 |= P4_AD_CAP_C|P4_AD_BAT;/*模拟*/
P4SEL1 |= P4_AD_CAP_C|P4_AD_BAT;
REFCTL0 |= REFVSEL_0; // Enable internal 1.2V reference
REFCTL0 &= ~REFON;
/* 初始化AD数据 */
ADC12CTL1 |= ADC12CONSEQ_0;
ADC12CTL0 &= ~ADC12ENC;
ADC12CTL0 &=~ADC12ENC;/*取消允许转换下面目的要设置*/
ADC12CTL1 = ADC12SHP/*使用采样和脉冲保持模式*/\
|ADC12CONSEQ_1 /*使用多通道单次采样功能*/
|ADC12SHS_0
|ADC12SSEL_0;
ADC12CTL2 = ADC12RES_2;/*12位转换结果*/
ADC12CTL3 = ADC12CSTARTADD_0;/*MEM0开始ADC12TCMAP内部温度采集使能*/
ADC12MCTL0 = ADC12VRSEL_4/*选择V+=verev=2.5V作为参考 V-=Vss*/\
|ADC12INCH_12/*选择A2通道->电场通道1->ADC12MEM0*/\
|ADC12EOS;
// ADC12MCTL1 = ADC12VRSEL_4|ADC12INCH_1; /* 参考电源采样 */
// ADC12MCTL2 = ADC12VRSEL_4/*选择V+=verev=2.5V作为参考 V-=Vss*/\
// |ADC12INCH_2/*选择A11通道->电场采样1->ADC12MEM6*/;
//
ADC12CTL0 = ADC12ON/*模块使能*/
|ADC12MSC
|ADC12ENC
|ADC12SHT1_1
|ADC12SHT0_1;/*多通道采样*/
}
A3通道
{
while(ADC12CTL1&ADC12BUSY); /* 等待采样结束 */
/* 初始化AD引脚 */
P1SEL0 |= P1_AD_I|P1_AD_U|P1_VEREF;/*模拟*/
P1SEL1 |= P1_AD_I|P1_AD_U|P1_VEREF;
P4SEL0 |= P4_AD_CAP_C|P4_AD_BAT;/*模拟*/
P4SEL1 |= P4_AD_CAP_C|P4_AD_BAT;
REFCTL0 |= REFVSEL_0; // Enable internal 1.2V reference
REFCTL0 &= ~REFON;
/* 初始化AD数据 */
ADC12CTL1 |= ADC12CONSEQ_0;
ADC12CTL0 &= ~ADC12ENC;
ADC12CTL0 &=~ADC12ENC;/*取消允许转换下面目的要设置*/
ADC12CTL1 = ADC12SHP/*使用采样和脉冲保持模式*/\
|ADC12CONSEQ_1 /*使用多通道单次采样功能*/
|ADC12SHS_0
|ADC12SSEL_0;
ADC12CTL2 = ADC12RES_2;/*12位转换结果*/
ADC12CTL3 = ADC12CSTARTADD_0;/*MEM0开始*/
ADC12MCTL0 = ADC12VRSEL_4/*选择V+=verev=2.5V作为参考 V-=Vss*/\
|ADC12INCH_3
|ADC12EOS/*选择A2通道->电流通道1->ADC12MEM0*/;
ADC12MCTL1 = ADC12VRSEL_4|ADC12INCH_1; /* 参考电源采样 */
ADC12MCTL2 = ADC12VRSEL_4/*选择V+=verev=2.5V作为参考 V-=Vss*/\
|ADC12INCH_2/*选择A11通道->电场采样1->ADC12MEM6*/;
ADC12CTL0 = ADC12ON/*模块使能*/
|ADC12MSC
|ADC12ENC
|ADC12SHT0_1;/*多通道采样*/
}
是要优化功耗,我在主函数中会进入LPM3低功耗模式,低功耗模式是已经进入了,不然不可能功能那么低。现在主要问题是不同通道功耗不同,即使在A12中加了停止还是不行,功耗还是比A3大十几个微安
就是不同通道下,在LPM状态下,A12功耗比A3高了十几个微安
引脚配置成AD状态,这个状态还需要配置上下来拉?
P1SEL0 |= P1_AD_I|P1_AD_U|P1_VEREF;/*模拟*/
P1SEL1 |= P1_AD_I|P1_AD_U|P1_VEREF;