Other Parts Discussed in Thread: MSP430F5438
请问MSP430F5438的A10通道ADC的采样误差大概是多少,另外例程在哪里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问MSP430F5438的A10通道ADC的采样误差大概是多少,另外例程在哪里?
例程在这个位置:C:\ti\msp\MSP430Ware_3_80_12_03\examples\devices\MSP430F5xx_6xx\MSP430F541xA_MSP430F543xA_Code_Examples
采样误差没有官方说明,这个跟你的参考电压有关。参考电压误差越小,采样误差也越小
你好,这个问题我咨询了一下美国工程师,收到回复如下:
The ADC accuracy should not be influenced by the temperature calibration. The temperature sensor though could vary based on that calibration, customers can use their own calibration data if they prefer. The ±3 is the range in the calibrations that have been done so a 85℃'s calibration could actually be at 83℃.