This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO-MSP: CCS无法安装MSP430和MSP432组件

Part Number: CCSTUDIO-MSP

当我运行CCS 11.0.0.00012安装程序时,无法安装MSP430或MSP432组件,报错只能退出。

报错信息如下:

CCS_ERROR: Unable to install repotype executable
D:\ti\ccs1100\ccs\eclipse\downloads\ti_msp430pack_setup64_11.0.0.exe: Error running
D:\ti\ccs1100\ccs\eclipse\downloadsiti_msp430pack_setup64_11.0.0.exe --prefix "D:\ticcs1100/ccs" --eclipseprefix "D:/ti/ccs1100/ccs/eclipse"--mode unattended --installer-log
"D:\ti\ccs1100/ccs/install_logs/20211206144329" --ccs true: child killed:unknown signal.
Do you want to retry?

There has been an error.Error running
D:\ti\ccs1100\ccs\eclipse\downloadsiti_msp430pack_setup64_11.0.0.exe --prefix "D:\ti\ccs1100/ccs" --eclipseprefix "D:/ti/ccs1100/ccs/eclipse"--mode unattended --installer-log
"D:\ti\ccs1100/ccs/install_logs/20211206151047"--ccs true: child killed:unknown signal
The application will exit now.

但是C2000组件是可以正常安装完成的。我的操作系统为Windows 11 专业版 Insider Preview Dev 22509.1011,在重装系统之前,这个安装文件是能够正常在之前的Windows 11上安装MSP430或MSP432组件的。

安装日志文件如下:

install_logs.zip