This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.工程环境
使用 MSP430FR2633芯片,CapTIvateDesignCenter软件生成的工程。使用UART的自动波特率模式来用作LIN通信。
2.有规定上电后100ms需要初始化完成,并能正常工作。但是发现时钟初始化时间过长 ,时钟初始化参考例程的,配置如下:
3.时钟初始化时间
在时钟初始化前后添加IO翻转,测量得出IO翻转间隔80ms.
请教一下应该如何快速启动,优化时钟初始化的时间?
您好,请您参阅https://www.ti.com/lit/an/slaa992/slaa992.pdf的第4.2节。
您可以在上电时从非易失存储器中加载DCO和FLL的相关参数,来达到快速锁定频率的目的。
好的,我先看看。现在需要调试MSP430FR2676,需要一个离线的烧录器,麻烦推荐一下,并给一下链接,谢谢