This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RTC模块需要外接晶振吗?
如果外接,要求精度多少ppm.
需要外接电容吗?
XinXin Li,
MSP430上的RTC分为以下三种,关于是否需要外接晶振请参考input clocks那行。当接32768Hz的晶体时,可以不接外部电容,因为MSP430内部设计有电容,可直接使用。
楼主你好!
1、RTC可以使用外部32.768khz晶振,也可以使用内部的32.768khz振荡器。负载电容可以使用外部的也可以使用内部的。
2、精度要求取决于应用对于精度的要求。
好像精度很低的样子
RTC的精度,仅与时钟源的精度有关系。
一般不需要,430自身的晶振精度也有5个ppm的。