This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【FAE分享】MSP430封装汇总贴,求封装的兄弟进,贡献封装的直接回复本帖。

MSP430系列MCU Altium designer 原理图、PCB封装。

下面是Billy哥的封装们:

1、MSP430F5310IRGC

http://www.deyisupport.com/cfs-file.ashx/__key/communityserver-discussions-components-files/55/3175.MSP430F5310IRGC.7z

2、MSP430F5310IPT

http://www.deyisupport.com/cfs-file.ashx/__key/communityserver-discussions-components-files/55/3276.MSP430F5310IPT.7z


Applications :

The MSP430 can be used for low powered embedded devices. The electric current drawn in idle mode can be less than 1 µA. The top CPU speed is 25 MHz. It can be throttled back for lower power consumption. The MSP430 also uses six different low-power modes, which can disable unneeded clocks and CPU. Additionally, the MSP430 is capable of wake-up times below 1 microsecond, allowing the microcontroller to stay in sleep mode longer, minimizing its average current consumption. The device comes in a variety of configurations featuring the usual peripherals: internal oscillator,timer including PWMwatchdogUSARTSPII²C, 10/12/14/16/24-bit ADCs, and brownout reset circuitry. Some less usual peripheral options include comparators (that can be used with the timers to do simple ADC), on-chip op-amps for signal conditioning, 12-bit DACLCD driver, hardware multiplierUSB, and DMA for ADC results. Apart from some older EPROM (MSP430E3xx) and high volume mask ROM(MSP430Cxxx) versions, all of the devices are in-system programmable via JTAG (full four-wire or Spy-Bi-Wire) or a built in bootstrap loader (BSL) using RS-232.