This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430AFE253: ADC设计问题与差分通道接地

Part Number: MSP430AFE253


设计一个直流电能量功率计,电压1000V 暂定电流1000A.电压采用分压电阻,电流采用75mv分流电阻FL-2

设计时参考官方交流电能表的设计,有几个疑问。

上图是,我设计的原理图。下图是MSP430AFE253官方DEMO。

                                        图2                                                                                                                                          图3

1.为什么VIN_P通道的 串联的电阻是100R ,其他通道是1K ,多个官方DEMO都是这样?

2.AGND的接地,VIN_M为什么要接地?是不是每个通道都接地?接地是不是因为有什么泄放电流的要求?

3.采样电阻通常都是采用开尔文接法,如果按照 第一张图 的R24 R25 (R26备用)接地,是不是就破坏了开尔文接线法。“高压-” 与 “电流-” 虽然是理论短路的,但是“电流-”是准备接在分流器专用触点上的,是不是电路只保留一个R24的接地就可以了?