Other Parts Discussed in Thread: MSP430F1611, MSP430G2221
UART spi模式下,spi时钟设置成4M时,主程序给txbuf一个字节时,spi接口却会连续重复发送两次该字节!
附测试程序,及SCK和SIMO波形图,求解释。
器件:MSP430F1611
IAR: 5.10
测试程序:
#include <msp430x16x.h>
void InitUART(void)
{
//时钟设置
BCSCTL1 &= ~XT2OFF; //开启8M时钟
BCSCTL2 += SELM_2; //设置MCLK为8M时钟输入
P3SEL |= BIT1 + BIT2 + BIT3;//0x3E; // P3.1,2,3,4,5 = USART0 SIMO, SOMI,UCLK
P3DIR |= BIT1 + BIT3 + BIT0;//0x1B; //
P3DIR &= ~BIT2;//
P3OUT |= BIT0; //
P5DIR |= BIT4;
P5OUT |= BIT4;
UCTL0 |= SWRST;
ME1 |= USPIE0; // Enable USART0 T/RXD
IE1 |= URXIE0; // enable interrupts
IE1 |= UTXIE0;
UCTL0 |= CHAR+SYNC+MM; // 8-bit character, SPI mode, Master
UTCTL0 |= SSEL1+STC+CKPL; // UCLK = SMCLK,3pin SPI mode
BCSCTL2 |= SELS + DIVS_0; //SMCLK = MCLK/1
UBR00 = 0x02;//0x20; // 8M/2=4M
UBR10 = 0x00; //
UCTL0 &= ~SWRST; // Initialize USART state machine
}
main( void )
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
InitUART();
while(1)
{
while (!(IFG1 & UTXIFG0)); //判断发送缓存是否为空
TXBUF0 = 0x01;
while (!(IFG1 & UTXIFG0)); //判断发送缓存是否为空
TXBUF0 = 0x0F;
}
}
主程序: spi轮流输出0x01,0x0F.
实测IO:
下图中,黄色信号为SCK,蓝色信号为SIMO。可以看到,从左到右SIMO依次传输数据为:0x0F,0x0F,0x01,0x01。

水平时基1us下的视图: