请问这个32MHz指的是?对于f5438a来说。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问这个意思是说CPU只能跑到25M而其他模块能用更高的频率么,或者说时钟系统支持32M晶振,但是给CPU用的时钟必须分频到25M以下后才能用
zq2,
按照数据手册,MCLK的确只能跑到25MHz (当然,一定范围内的超频是允许的,但是不建议这么做,当你倍频超过系统承受的频率的时候,系统是不能正常工作的。), 但是时钟系统的外部晶体输入可以支持高达32MHz, FLL控制的DCO输出最高可达135MHz, 但是CPU的MCLK的时钟源无论是从DCO,XT1还是XT2来,分频后最好降到25Mhz以下。
其他模块可以使用的时钟源一般不会超过系统时钟,即不会超过主频,具体参数参见数据手册。
希望对你有帮助!O(∩_∩)O~