/*
* AD_main.c
*
* Created on: 2013-8-4
* Author: Administrator
*/
#include<msp430f5529.h>
#include"HAL_Board.h"
#define num_results 512
int results[num_results] = {0};
void ADC_Init(void);
void main(void)
{
WDTCTL=WDTPW+WDTHOLD;//关闭看门狗
Board_init(); //初始化GPIO
ADC_Init();//ADC初始化
ADC12CTL0 |=ADC12ENC;//AD转换允许
LPM0;//进入低功耗模式0
}
void ADC_Init(void)
{
P8DIR |=BIT1;//P8.1为输出,即led2
P8OUT &=~BIT1;//led2灭
P6SEL |=BIT0;//打开AD模拟端口A0
//配置ADC12
ADC12CTL0 = ADC12ON+ADC12SHT02+ADC12REF2_5V+ADC12REFON ;
//打开ADC12内核,采样保持时间系数2,选择内部参考电压2.5v,打开内部参考电压发生器
ADC12CTL1 = ADC12SHP+ADC12CONSEQ_2+ADC12SHS_1;
//采样定时器作为采样触发信号源SAMPCON,由采样输入信号ADC12CLK的上升沿触发采样定时器
//单通道多次采样,采样触发源为TIMERA的输出单元out1输出的信号(由CCR1定时产生)
ADC12MCTL0 =ADC12INCH_0+ADC12SREF_1;
//选择0通道,参考电压源为:v+=Vref+,v-=Avss
ADC12IE |=BIT0;//开中断允许ADC12IFG.0
//配置定时器
TA0CCR0 =1500;//延时
TA0CCTL0 |=CCIE;//开定时器中断允许,定时器为比较模式
TA0CTL = TASSEL_1 | MC_1;//TACLK=ACLK,增计数模式
LPM3;
TA0CCTL0 &=~CCIE;//关闭定时器捕获比较中断
P1SEL |=BIT2;//开TA0.1作为TIMERA_out1的输出功能
P1DIR |=BIT2;//输出
TA0CCR0 = 7;//初始化TA0CCL0,采样时钟周期=CCR0+1
TA0CCR1 = 4;
//初始化TA0CCL1,用于产生一个TIMERA_out1信号给ADC12做采样触发信号源
TA0CCTL1 =OUTMOD_3;
//CCR1捕获比较寄存器的out1输出单元为置位/复位模式
TA0CTL =TACLR | MC_1 |TASSEL_1;
//清除TA,增计数模式,定时器时钟为ACLK
}
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR(void)
{
static unsigned int index =0; //静态变量
switch(__even_in_range(ADC12IV,34))
{
case 0: break; // Vector 0: No interrupt
case 2: break; // Vector 2: ADC overflow
case 4: break; // Vector 4: ADC timing overflow
case 6: // Vector 6: ADC12IFG0
results[index++]=ADC12MEM0;//移动ADC结果到数组,此时ADC12IFG.0自动复位
if(index==512)
{
ADC12CTL0 &=~ADC12ENC;// 停止转换
index=0;
P8OUT |=BIT1;
LPM3;
}
case 8: break; // Vector 8: ADC12IFG1
case 10: break; // Vector 10: ADC12IFG2
case 12: break; // Vector 12: ADC12IFG3
case 14: break; // Vector 14: ADC12IFG4
case 16: break; // Vector 16: ADC12IFG5
case 18: break; // Vector 18: ADC12IFG6
case 20: break; // Vector 20: ADC12IFG7
case 22: break; // Vector 22: ADC12IFG8
case 24: break; // Vector 24: ADC12IFG9
case 26: break; // Vector 26: ADC12IFG10
case 28: break; // Vector 28: ADC12IFG11
case 30: break; // Vector 30: ADC12IFG12
case 32: break; // Vector 32: ADC12IFG13
case 34: break; // Vector 34: ADC12IFG14
default: break;
}
}
这是参考教程的例子写的,哪里出错?求大神指导!!!