This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMA将ADC12的数据不能传到乘法器中?



DMACTL0 =DMA0TSEL_24+DMA1TSEL_24;
DMACTL4 = DMARMWDIS;
__data16_write_addr((unsigned short) &DMA0SA,(unsigned long) &ADC12MEM0); //DMA0 目的地址
__data16_write_addr((unsigned short) &DMA0DA,(unsigned long) &MPY); //DMA0源地址
DMA0SZ=1; // DMA0 size = 1
DMA0CTL = DMADT_4+DMAEN+DMADSTBYTE+DMASRCBYTE; //


__data16_write_addr((unsigned short) &DMA1SA,(unsigned long) &ADC12MEM1); //DMA1 目的地址
__data16_write_addr((unsigned short) &DMA1DA,(unsigned long) &OP2); //DMA1源地址
DMA1SZ=1; // DMA1 size = 1
DMA1CTL = DMADT_4+DMAEN+DMADSTBYTE+DMASRCBYTE;

ADC12MEM0和ADC12MEM1中已经采集到了数据,但是DMA不能将数据传递到MPY和OP2中,MDA代码如上。

  •   // Setup DMA0
      DMACTL0 = DMA0TSEL_24;                    // ADC12IFGx triggered
      DMACTL4 = DMARMWDIS;                      // Read-modify-write disable
      DMA0CTL &= ~DMAIFG;
      DMA0CTL = DMADT_4+DMAEN+DMADSTINCR_3+DMAIE; // Rpt single tranfer, inc dst, Int
      DMA0SZ = 1;                               // DMA0 size = 1

      __data16_write_addr((unsigned short) &DMA0SA,(unsigned long) &ADC12MEM0);
                                                // Source block address
      __data16_write_addr((unsigned short) &DMA0DA,(unsigned long) &DMA_DST);
                                                // Destination single address

    参见这个例程,希望对你有所帮忙。

  • 你好!你说的这个代码我已经看过,但是有个问题:当我把ADC12的转换模式改为ADC12CONSEQ_2(单通道序列转换)就可以将ADC12MEN0的值转移到MPY中区,但是当我将ADC12转换模式改为ADC12CONSEQ_3(序列通道序列转换)时,DMA就不能将ADC12MEM0传到MPY,也不能将ADC12MEM1传到OP2中。不知道是什么原因?希望您能够再详细的讲解哈!谢谢!