This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我在使用LaunchPad msp430g2553的硬件I2C的时候遇到很多问题。我把CCSV5中提供的读PCF8574的历程下到板子上之后没有办法使用,上拉电阻我也接了,历程一点也没有改,已经确定硬件没有问题,但还是没法用,有谁能给我提供一个可以使用的历程或者是告诉我在使用硬件I2C的时候应该如何配置以及需要注意些什么问题吗?谢谢~\(≧▽≦)/~啦啦啦
Hello,
我觉得还是IIC没有配置好的原因。
你可以下载MSP430WARE软件库在里面找到需要的430所有的参考代码。
如果你已经下载CCS,那么在CCS View ->TI resource 里面可以找到 MSP430WARE 插件
下面是我在里面找到的一个关于总线IIC读取外部ADC数据的例程供你参考:
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430G2xx3 Demo - USCI_B0 I2C Master Interface to DAC8571, Write
//
// Description: Using UCB0TXIE, a continuous sine wave is output to the
// external DAC using a 16-point look-up table. Only one start condition
// is executed. Data is handled by the ISR and the CPU is normally in LPM0.
// ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.2MHz
//
// MSP430G2xx3 DAC8571
// ------------------ ------------
// -|XIN P1.7/UCB0SDA|<--------------->|SDA |
// | P1.6/UCB0SCL|---------------->|SCL I2C |
// -|XOUT | | SLAVE |
// | I2C MASTER | GND|A0 |
//
//
// DAC8571 I2C address = 0x4C (A0 = GND)
//
// D. Dang
// Texas Instruments Inc.
// February 2011
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430.h>
const unsigned char Sine_Tab[] = // 16 Point 16-bit Sine Table
{
0xFF, // MSB Word 0
0xFF, // LSB
0xF6, // MSB Word 1
0x40, // LSB
0xDA, // MSB Word 2
0x81, // LSB
0xB0, // MSB Word 3
0xFA, // LSB
0x7F, // MSB Word 4
0xFF, // LSB
0x4F, // MSB Word 5
0x03, // LSB
0x25, // MSB Word 6
0x7C, // LSB
0x09, // MSB Word 7
0xBD, // LSB
0x00, // MSB Word 8
0x00, // LSB
0x09, // MSB Word 9
0xBD, // LSB
0x25, // MSB Word 10
0x7C, // LSB
0x4F, // MSB Word 11
0x03, // LSB
0x7F, // MSB Word 12
0xFE, // LSB
0xB0, // MSB Word 13
0xFA, // LSB
0xDA, // MSB Word 14
0x81, // LSB
0xF6, // MSB Word 15
0x40 // LSB
};
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop Watchdog Timer
P1SEL |= BIT6 + BIT7; // Assign I2C pins to USCI_B0
P1SEL2|= BIT6 + BIT7; // Assign I2C pins to USCI_B0
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 12; // fSCL = SMCLK/12 = ~100kHz
UCB0BR1 = 0;
UCB0I2CSA = 0x4c; // Set slave address
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
IE2 |= UCB0TXIE; // Enable TX ready interrupt
UCB0CTL1 |= UCTR + UCTXSTT; // I2C TX, start condition
UCB0TXBUF = 0x010; // Write DAC control byte
__bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts
}
// USCI_B0 Data ISR
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
{
static unsigned char ByteCtr;
UCB0TXBUF = Sine_Tab[ByteCtr++]; // Transmit data byte
ByteCtr &= 0x1f; // Do not exceed table
}
如果你确实没有更改例程代码,建议你从硬件方面检查问题。下面给你列个如何查找问题的思路。你可以按照下面一条一条地对照操作。看问题处在第几步。
1. i2c的sda和scl口线需要有10-20k上拉电阻。(这点你已经确定了)
2. 断开从机,初始化i2c模块,用示波器看sda和scl口线电平,这个时候两个口线应该是高电平。
3. 连接从机在测量sda和scl的电平,如果这个时候口线保持为高就没问题,如果变低了,就说明从机有问题。
4. 断点设置到发送start之后, 用示波器观察信号是否能正确发出。
5. 断点设置到发送一个数据之后,用示波器观察是否有一字节数据发出,第9位是否为低电平。